2018-10-28 4:49 AM
with the help of the HAL code library i am able to see the output while using LOOPBACK mode in CAN but at the same time not able to get the data in the NORMAL mode . can any one help me out with this problem ?
thanks in advanced
2018-10-28 5:15 AM
You must have a terminator if you are using the line driver.
if you are not using a line driver you may need to pull up the line.
and you need a slave on the wire to respond.
also ABOM should be enabled,
2018-10-28 5:20 AM
thanks for your answer but firstly i want to check the protocol with two stm boards only that mean i want to do loopback by shorting the two board tx and rx pins in that one function name HAL_CAN_GetRxFifoFillLevel i am stucking it is not coming out with that function .
and ya already enable the ABOM as you said .so guide me what i have to do now ?
thanks you
2018-10-28 6:40 AM
you can't just join Rx to Tx
You have to join both the Rx pins together and use a pull up like 1k cause you are being dodgy..
Each of the Tx pins require a diode to pull down the joined Rx pins.
That is dodgy... but it works...
2018-10-28 6:43 AM
You'd need one of the nodes to receive/acknowledge the packets.
Aren't there some Network examples amongst the Cube trees for assorted chips/boards
2018-10-28 6:43 AM
it is not trivial to get this stuff running, do you have a scope ?
I purchased a CanDo unit from the UK,
I set it to transmit 1 packet every second, I worked on the receiver first.
It took a week to get 250khz running. Then I worked on the transmitter, it was done in a day.
2018-10-29 1:34 AM
with the help of the transceiver also i am not getting data .
and no there are no examples for the STM32L452RE-P if you have any working code kindly attached
thank you
2018-10-29 1:44 AM
ok i will try thank you
2018-10-29 3:06 AM
sorry but not getting what you are trying to say .
and ya here is my code for the board please check and let me know
i named a function CAN_Polling() for the CAN transmit and receive .
HAL_StatusTypeDef CAN_Polling(void)
{
CAN_FilterTypeDef sFilterConfig;
/*##-1- Configure the CAN peripheral #######################################*/
CanHandle.Instance = CAN1;
CanHandle.Init.TimeTriggeredMode = DISABLE;
CanHandle.Init.AutoBusOff = ENABLE;
CanHandle.Init.AutoWakeUp = DISABLE;
CanHandle.Init.AutoRetransmission = ENABLE;
CanHandle.Init.ReceiveFifoLocked = DISABLE;
CanHandle.Init.TransmitFifoPriority = DISABLE;
CanHandle.Init.Mode = CAN_MODE_NORMAL;
CanHandle.Init.SyncJumpWidth = CAN_SJW_1TQ;
CanHandle.Init.TimeSeg1 = CAN_BS1_6TQ;
CanHandle.Init.TimeSeg2 = CAN_BS2_2TQ;
CanHandle.Init.Prescaler = 5;
if(HAL_CAN_Init(&CanHandle) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
/*##-2- Configure the CAN Filter ###########################################*/
sFilterConfig.FilterBank = 0;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfig.FilterIdHigh = 0x0000;
sFilterConfig.FilterIdLow = 0x0000;
sFilterConfig.FilterMaskIdHigh = 0x0000;
sFilterConfig.FilterMaskIdLow = 0x0000;
sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
sFilterConfig.FilterActivation = ENABLE;
sFilterConfig.SlaveStartFilterBank = 14;
if(HAL_CAN_ConfigFilter(&CanHandle, &sFilterConfig) != HAL_OK)
{
/* Filter configuration Error */
Error_Handler();
}
/*##-3- Start the CAN peripheral ###########################################*/
if (HAL_CAN_Start(&CanHandle) != HAL_OK)
{
/* Start Error */
Error_Handler();
}
/*##-4- Start the Transmission process #####################################*/
TxHeader.StdId = 0x11;
TxHeader.RTR = CAN_RTR_DATA;
TxHeader.IDE = CAN_ID_STD;
TxHeader.DLC = 2;
TxHeader.TransmitGlobalTime = DISABLE;
// TxData[8]=(uint8_t *)"afflaffl";
TxData[0] = '1';
TxData[1] = '2';
/* Request transmission */
if(HAL_CAN_AddTxMessage(&CanHandle, &TxHeader, TxData, &TxMailbox) != HAL_OK)
{
/* Transmission request Error */
Error_Handler();
}
/* Wait transmission complete */
while(HAL_CAN_GetTxMailboxesFreeLevel(&CanHandle) != 3) {}
/*##-5- Start the Reception process ########################################*/
if(HAL_CAN_GetRxFifoFillLevel(&CanHandle, CAN_RX_FIFO0) != 1)
{
/* Reception Missing */
Error_Handler();
}
if(HAL_CAN_GetRxMessage(&CanHandle, CAN_RX_FIFO0, &RxHeader, RxData) != HAL_OK)
{
/* Reception Error */
Error_Handler();
}
if((RxHeader.StdId != 0x11) ||
(RxHeader.RTR != CAN_RTR_DATA) ||
(RxHeader.IDE != CAN_ID_STD) ||
(RxHeader.DLC != 2) )
// ((RxData[0]<<8 | RxData[1]) != 0x))
{
/* Rx message Error */
return HAL_ERROR;
}
return HAL_OK; /* Test Passed */
}
2018-10-29 3:14 AM
hello Clive
here is my initialization code for the CAN can you let me know what is the problem exactly and ya i connected the tx pin of controller to tx pin of transceiver and rx pin to rx same for the other node but not getting data could you please help.
thank you
HAL_StatusTypeDef CAN_Polling(void)
{
CAN_FilterTypeDef sFilterConfig;
/*##-1- Configure the CAN peripheral #######################################*/
CanHandle.Instance = CAN1;
CanHandle.Init.TimeTriggeredMode = DISABLE;
CanHandle.Init.AutoBusOff = ENABLE;
CanHandle.Init.AutoWakeUp = DISABLE;
CanHandle.Init.AutoRetransmission = ENABLE;
CanHandle.Init.ReceiveFifoLocked = DISABLE;
CanHandle.Init.TransmitFifoPriority = DISABLE;
CanHandle.Init.Mode = CAN_MODE_NORMAL;
CanHandle.Init.SyncJumpWidth = CAN_SJW_1TQ;
CanHandle.Init.TimeSeg1 = CAN_BS1_6TQ;
CanHandle.Init.TimeSeg2 = CAN_BS2_2TQ;
CanHandle.Init.Prescaler = 5;
if(HAL_CAN_Init(&CanHandle) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
/*##-2- Configure the CAN Filter ###########################################*/
sFilterConfig.FilterBank = 0;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfig.FilterIdHigh = 0x0000;
sFilterConfig.FilterIdLow = 0x0000;
sFilterConfig.FilterMaskIdHigh = 0x0000;
sFilterConfig.FilterMaskIdLow = 0x0000;
sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
sFilterConfig.FilterActivation = ENABLE;
sFilterConfig.SlaveStartFilterBank = 14;
if(HAL_CAN_ConfigFilter(&CanHandle, &sFilterConfig) != HAL_OK)
{
/* Filter configuration Error */
Error_Handler();
}
/*##-3- Start the CAN peripheral ###########################################*/
if (HAL_CAN_Start(&CanHandle) != HAL_OK)
{
/* Start Error */
Error_Handler();
}
/*##-4- Start the Transmission process #####################################*/
TxHeader.StdId = 0x11;
TxHeader.RTR = CAN_RTR_DATA;
TxHeader.IDE = CAN_ID_STD;
TxHeader.DLC = 2;
TxHeader.TransmitGlobalTime = DISABLE;
// TxData[8]=(uint8_t *)"afflaffl";
TxData[0] = '1';
TxData[1] = '2';
/* Request transmission */
if(HAL_CAN_AddTxMessage(&CanHandle, &TxHeader, TxData, &TxMailbox) != HAL_OK)
{
/* Transmission request Error */
Error_Handler();
}
/* Wait transmission complete */
while(HAL_CAN_GetTxMailboxesFreeLevel(&CanHandle) != 3) {}
/*##-5- Start the Reception process ########################################*/
if(HAL_CAN_GetRxFifoFillLevel(&CanHandle, CAN_RX_FIFO0) != 1)
{
/* Reception Missing */
Error_Handler();
}
if(HAL_CAN_GetRxMessage(&CanHandle, CAN_RX_FIFO0, &RxHeader, RxData) != HAL_OK)
{
/* Reception Error */
Error_Handler();
}
if((RxHeader.StdId != 0x11) ||
(RxHeader.RTR != CAN_RTR_DATA) ||
(RxHeader.IDE != CAN_ID_STD) ||
(RxHeader.DLC != 2) )
// ((RxData[0]<<8 | RxData[1]) != 0x))
{
/* Rx message Error */
return HAL_ERROR;
}
return HAL_OK; /* Test Passed */
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.