STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407 USB FS Device mode Programing

Hi. I am using STM32F407 discovery board programed in USB FS mode. The driver used is WINUSB. mY os IS WINDOWS 10. I am using USF FS configured as ENDP1 OUT and ENDP1 IN. Both in bulk mode. I was managed to successfully enumerated with PC an...

CAN TX ERRORS ??? please help

Hellofollowing the CAN lectures I have a real strange problem transmitting can messageI have two can nodes 1) nucleo 446re board and node 2) is my Can Bus AnalyserI even get the same TX errors in loop back mode & Can normal mode ????why ?? what is wr...

0690X000006CTNWQA4.jpg 0690X000006CTNMQA4.jpg 0690X000006CTNHQA4.jpg 0690X000006CTOPQA4.jpg
JHERI by Senior
  • 1633 Views
  • 0 replies
  • 0 kudos

BOOT0 behavior

Hello!i would like to understand what happens to BOOT0 during the run of regular program (not bootloader).What will happen if i set it to '1' or reset it to '0' during the run?​

YuriCh by Associate II
  • 970 Views
  • 1 replies
  • 0 kudos

stm32f469 PWN not output NState ?

My project needs to output PWM NState, My code is as follows, but no PWM signal output has been detected by the oscilloscope measurement. How can I solve this problem? #define MOTOR_DE_RCC_PERIPH RCC_AHB1Periph_GPIOC #define MOTOR_DE_PORT...

ac.2 by Associate II
  • 753 Views
  • 0 replies
  • 0 kudos

How to change to com port?

When connecting the 32L152C-Discovery board, it looks like STLink Dongle.​ How do I change the STLink Dongle to COM PORT?

0690X000006CTL1QAO.jpg
ngabj by Associate
  • 1040 Views
  • 1 replies
  • 0 kudos

Trying to design pcb with STM32F446RE, got some questions.

Hey! i just jumped from AVR8bit MCU's to STM32 and obviously i'm having issues with just about everything when it comes to design PCB, i try to keep it short.Boot0 and Boot1 pins should be jumpered to give me access to bootloader right?(regardless if...

JoniS by Senior
  • 1299 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.