2018-11-24 8:32 PM
My project needs to output PWM NState, My code is as follows, but no PWM signal output has been detected by the oscilloscope measurement. How can I solve this problem?
#define MOTOR_DE_RCC_PERIPH RCC_AHB1Periph_GPIOC
#define MOTOR_DE_PORT GPIOC
#define MOTOR_DE_PIN GPIO_Pin_6
#define MOTOR_PWM_RCC_PERIPH RCC_AHB1Periph_GPIOC
#define MOTOR_PWM_TIMER_PERIPH RCC_APB2Periph_TIM8
#define MOTOR_PWM_PORT GPIOC
#define MOTOR_PWM_PIN GPIO_Pin_7
#define MOTOR_PWM_AF GPIO_AF_TIM8
#define MOTOR_PWM_TIM TIM8
#define MOTOR_PWM_PIN_SOURCE GPIO_PinSource7
#define PWM_FREQ 100 // 100 Hz
#define PWM_INITIAL_PULSE 1000
void bsp_motor_output_nstate (void)
{
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
uint16_t usPeriod;
uint16_t usPrescaler;
uint32_t uiTIMxCLK;
// enable GPIO clock
if(MOTOR_PWM_RCC_PERIPH == MOTOR_DE_RCC_PERIPH)
{
RCC_AHB1PeriphClockCmd(MOTOR_DE_RCC_PERIPH, ENABLE);
}
else
{
RCC_AHB1PeriphClockCmd(MOTOR_DE_RCC_PERIPH, ENABLE);
RCC_AHB1PeriphClockCmd(MOTOR_PWM_RCC_PERIPH, ENABLE);
}
//configure GPIO
GPIO_InitStructure.GPIO_Pin = MOTOR_DE_PIN;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_Init(MOTOR_DE_PORT, &GPIO_InitStructure);
GPIO_WriteBit(MOTOR_DE_PORT, MOTOR_DE_PIN, Bit_RESET);
/* confiure motor PWM timer */
// enable tiemr clk
RCC_APB2PeriphClockCmd(MOTOR_PWM_TIMER_PERIPH, ENABLE);
//configure GPIO
GPIO_InitStructure.GPIO_Pin = MOTOR_PWM_PIN;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ;
GPIO_Init(MOTOR_PWM_PORT, &GPIO_InitStructure);
// link to AF function
GPIO_PinAFConfig(MOTOR_PWM_PORT, MOTOR_PWM_PIN_SOURCE, MOTOR_PWM_AF);
// configure PWM Freq
uiTIMxCLK = SystemCoreClock;
if(PWM_FREQ < 100)
{
usPrescaler = 10000 - 1;
usPeriod = (uiTIMxCLK / 10000) / PWM_FREQ - 1;
}
else if(PWM_FREQ < 3000)
{
usPrescaler = 100 - 1;
usPeriod = (uiTIMxCLK / 100) / PWM_FREQ - 1;
}
else
{
usPrescaler = 0;
usPeriod = uiTIMxCLK / PWM_FREQ - 1;
}
// Time base configuration
TIM_TimeBaseStructure.TIM_Period = usPeriod;
TIM_TimeBaseStructure.TIM_Prescaler = usPrescaler;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseStructure.TIM_RepetitionCounter = 0x0000; // TIM1 and TIM8 must setting
TIM_TimeBaseInit(MOTOR_PWM_TIM, &TIM_TimeBaseStructure);
// PWM1 Mode configuration: Channel2
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Disable;
TIM_OCInitStructure.TIM_Pulse = (PWM_INITIAL_PULSE * usPeriod) / 10000;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Enable; // only for TIM1 and TIM8.
TIM_OCInitStructure.TIM_OCNPolarity = TIM_OCNPolarity_High; // only for TIM1 and TIM8.
TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Reset; // only for TIM1 and TIM8.
TIM_OCInitStructure.TIM_OCNIdleState = TIM_OCNIdleState_Reset; // only for TIM1 and TIM8.
TIM_OC2Init (MOTOR_PWM_TIM, &TIM_OCInitStructure);
TIM_OC2PreloadConfig(MOTOR_PWM_TIM, TIM_OCPreload_Enable);
TIM_ARRPreloadConfig(MOTOR_PWM_TIM, ENABLE);
// TIMx enable counter
TIM_Cmd (MOTOR_PWM_TIM, ENABLE);
TIM_CtrlPWMOutputs (MOTOR_PWM_TIM, ENABLE);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.