STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hello, guys! I have problem with STM32L0 ADC. I measure VrefInt voltage but the behaviour of the ADC is not stable - it reports corect values(4095) alongside with incorrect values (1950)?! Would you please help me.

Initialization:static void MX_ADC_Init(void){ ADC_ChannelConfTypeDef sConfig;  /**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)  */ hadc.Instance = ADC1; hadc.Init.OversamplingMode = DISABLE; ha...

LMehm by Associate III
  • 1344 Views
  • 2 replies
  • 0 kudos

Encoder Interface on TIM2-TIM5

Posted on November 20, 2012 at 15:48Hello, I am having difficulty configuring the quadrature encoder interface on timers 2 through 5.  I have successfully configured the encoder interface on timers 1 and 8, using the code below: TIM_TimeBaseInitType...

Resolved! DMA1, 2 and DMAMUX - how to do it?

Hello,I am porting a project from STM32F4 to STM32H7. This project uses DMA1 and DMA2 with timer 8 and DAC and it works fine on STM32F4 but I can't get DMA running on STM32H7. Up to now I understood it this way that all I have to do is set the right ...

What‘s the actual GBW of OPAMP in STM32F303?

(yellow line: non inverting inputblue line: output of OPAMP )Hi,I am using the NUCLEO-F303RE board and now I am testing the OPAMP3 , which is one of the peripherals in STM32F303. I have set the PA1 as non inverting input, PB2 as inverting input. And...

0690X000006CTW4QAO.bmp
KMak by Associate
  • 1027 Views
  • 1 replies
  • 1 kudos

SPI frame longer than 16 bits with stm32f103

Hi,I need to perform write and read operations on an external flash memory through spi protocol.The spi peripheral in the stm32f103 can be configured to 8 or 16 bits data frame lenght. I would like to be able to send longer frames. Is it a possible s...

abcdef by Associate
  • 875 Views
  • 0 replies
  • 0 kudos

Hardfault on IAP jump to APP

Hi guys,I have use the stm32f105 to do a job on the IAP jump tp APP, and normally it works fine, but latest day, I have to disable the USB code on the APP code, then use the flash download demonstrator to download the APP, it runs OK, and then re-pow...

cable gu by Associate II
  • 5434 Views
  • 10 replies
  • 0 kudos

SW4STM32 variables for AC6 version of openocd

I've run SW4STM32 for the last 2 years with an external openocd package but I see that the AC6 version has recently been updated so I thought I'd try it. It gets stored in ~/.p2/pool/plugins/fr.ac6.mcu.externaltools.openocd.linux64_1.21.0.20181113124...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.