STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Application start address can be != start of flash ?

Hello,I need to use the example which boots (jumps) into application in external memory, but with a very slight modification:So that the start address of application can be somewhere inside the flash, not particulary at the start of flash, as it is n...

ranran by Senior II
  • 1488 Views
  • 2 replies
  • 0 kudos

Core peripherals?

Where, in the documentation of STM32 devices, can I find out which optional core peripherals are implemented?

USB FS speed vs USB HS with internal FS Phy with DMA

I have a custom board using a STM32F446RET6 with a SDCard. It is configuredbe a mass storage device and use USB_OTG_FS. I read another post where someone mentioned the STM32F4 can use USB HS but usethe Internal FS Phy. The advantage to doing this is ...

STM32H7 -FMC - LCD INTEFACE - A19 AS REGISTER SELECT

Hi, When A0 is used as Register select in the FMC LCD interface, ST uses the code below: typedef struct{ __IO uint16_t REG; __IO uint16_t RAM;}LCD_CONTROLLER_TypeDef;/* We use BANK1 as we use FMC_NE1 signal */#define FMC_BANK1_BASE ((uint32_t)(0x...

Asantos by Senior
  • 1263 Views
  • 4 replies
  • 0 kudos

I can't get data from CAN

Hi everyone,I'm new using ST microcontrollers and I've began using blue pill development board. My project has to read data from CAN at 250 kb/s. Also I'm using MikroC PRO for ARM to create the program but I'm unable to read any data from CAN so far....

Dayi by Associate
  • 1864 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.