2018-12-04 6:25 AM
I have a custom board using a STM32F446RET6 with a SDCard. It is configured
be a mass storage device and use USB_OTG_FS.
I read another post where someone mentioned the STM32F4 can use USB HS but use
the Internal FS Phy. The advantage to doing this is the USB_OTG_HS can use
DMA.
I can get around 700Kbs to 800Kbs transfer speeds using USB_OTG_FS but would
like to know if changing the configuration to use USB_OTG_HS but with the
Internal FS Phy and DMA gives any noticeable speed increases.
Thanks for any information.
2018-12-04 7:47 AM
>>I can get around 700Kbs to 800Kbs transfer speeds using USB_OTG_FS but would like to know if changing the configuration to use USB_OTG_HS but with the Internal FS Phy and DMA gives any noticeable speed increases.
No, I think that's about the ceiling on 12Mbps
2018-12-04 3:32 PM
Ok, I won't bother making changes to test it.
Thank you Clive.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.