STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F746-DISCO + openocd + gdb + eclipse

Posted on July 03, 2018 at 15:21Hello,I have plenty of problems to debug on STM32F746-DISCO with openocd and eclipseThe most frequent is that, just after programming the Flash, the MCU goes directly on the Hard fault handler, and does not even go to...

Resolved! USART3_IRQHandler is not invoked.

char recv_string[10];char data;int count = -1,i,data_check = -1;void USART3_IRQHandler(void) //my interrupt handler{ if(USART_GetITStatus(USART3,USART_IT_TXE)) { data = USART_GetChar(); if(data == 0x0D || data == 0x08) data_check = 1; e...

psati by Associate II
  • 2302 Views
  • 2 replies
  • 0 kudos

UART interrupt lost

Under FREERTOS on UART3, I receive a 40 byte packet every 2.5ms @ 921600 baud . I programmed the Rx FIFO to interrupt at 1/2 level threshold. Everything works fine for about an hour. Then, for some reason, I get an overrun condition which seems to me...

DMose by Associate
  • 1044 Views
  • 1 replies
  • 0 kudos

STM32F072C8 CANBUS Loopback working but Normal mode isnt.

Hi I am hoping someone can help me with a frustrating problem. I have two boards setup with STM32F072C8 parts. I have downloaded the examples from ST which are for a larger footprint part and modified the code to run on the 48 pin parts. The loopback...

r9rej by Associate
  • 868 Views
  • 0 replies
  • 0 kudos

execution time-STM32F429zi

i am just executing a for loop of 4096 time. But it takes more than 1 ms in stm32f429zi series. Clock frequency is 180MHz. How it can take that much time or whether it is executing some other function in back end.

SR.6 by Associate
  • 1104 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.