STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

QuadSPI Single SPI mode IO2 state

In Single SPI mode, the unused qspi pins are held as follows: IO2 is in output mode and forced to ‘0’ (to deactivate the “write protect�? function) IO3 is in output mode and forced to ‘1’ (to deactivate the “hold�? function)Problem is, all the flash ...

I2C slave transmit in interrupt mode

Hi all,I do have a problem with I2C slave transmit mode. Everytime the master (in my case an FTDI FT4222) starts a read access I get the error ACKNOLEDGE FAILURE.If I just transmit from a PC to the STM32 everything works fine and I receive the correc...

0690X000006D9aoQAC.png 0690X000006D9bNQAS.png
SZank by Associate II
  • 1102 Views
  • 0 replies
  • 0 kudos

Resolved! How to read gpio using dma in Input Capture mode

Hi,I want to  configure the DMA so that it transfers data from the GPIO lines (8 bit data lines) to the RAM buffer upon receiving a trigger signal on the timer capture input channel TIM1_CHI (PE9) . I am using stm32f446ze.We nees to acquire data regi...

Amal Babu by Associate III
  • 6211 Views
  • 8 replies
  • 0 kudos

Early waking Up from STOP mode

Dear,I use SM32L152, I go to STOP mode regularly and as the possible source of waking up is either RTC or External interrupt. It works Fine until I change the System clocks from MSI 4 MHz to for example HSI on 16 MHz. If I change it, then MY MCU is w...

JAN R by Associate III
  • 3585 Views
  • 8 replies
  • 0 kudos

UART DMA TX/Rx problem w/ STM32F722 example

Posted on February 14, 2018 at 01:55Hello,I have a program using serial UART communicatons. I based the UART code on the example code UART_TwoBoards_ComDMA.  The system seems to work correctly when it is in command/response mode.  That means, I can ...

Reading 2 ADC Channels and Outputting Over USART

I'm new to working with STM32's so if I make any mistakes please let me know. I have the STM32F446RE Nucleo board and I'm trying to read two ADC channels (IN15 on GPIOC_05 and IN14 on GPIOC_04) and output the ADC values over USART 1 channel as fast ...

0690X000006D92mQAC.png
PAbdu by Associate II
  • 1913 Views
  • 4 replies
  • 0 kudos

DMA Tx stream FIFO error in SPI slave - How do I fix it?

I am working with the STM32F769NIH6 microcontroller and it's communicating with a different processor using a home-made SPI-based protocol where the STM32F769NIH6 is the slave. The master clocks data at 11 MHz and the STM32F769NIH6 is running at 120 ...

arnold_w by Senior II
  • 1261 Views
  • 3 replies
  • 0 kudos

How to flash custom Sigfox credentials

Hi,I am working on a custom device, based on Murata CMWX1ZZABZ, running both Sigfox and LoRa.Regarding Sigfox, I would like to use my own Sigfox Credentials, acquired direclty from Sigfox (not from Murata). However, the only documented process I can...

Slan by Associate II
  • 2145 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.