2019-02-04 1:26 AM
Hi everyone.
I'm trying to setup TIM2_CH4 remapped as input capture, in order to detect rising edges on PB11.
I'm working with HALs. And my code is next:
First of all, for initialization:
// APB2 (which is 64 MHz) at 8 MHz
timer_cap_timhandle_.Instance = TIMx;
timer_cap_timhandle_.Init.Period = 0;
timer_cap_timhandle_.Init.Prescaler = 7;
timer_cap_timhandle_.Init.ClockDivision = TIM_CLOCKDIVISION_DIV4;
timer_cap_timhandle_.Init.CounterMode = TIM_COUNTERMODE_UP;
timer_cap_timhandle_.Init.RepetitionCounter = 0;
timer_cap_timhandle_.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
// ---------------------------
// Setup low level resources
TIMx_CLK_ENABLE();
//Interrupt priority
HAL_NVIC_SetPriority(TIMx_IRQn, 0, 0);
//Enable TIM2 interrupts
HAL_NVIC_EnableIRQ(TIMx_IRQn);
//Enable GPIOA timer
__HAL_RCC_GPIOA_CLK_ENABLE();
//Setup timer_cap and its handler
if(HAL_TIM_IC_Init(&timer_cap_timhandle_) != HAL_OK)
{
//Error
return -1;
}
//Remap I/O ports for TIM2
__HAL_AFIO_REMAP_TIM2_ENABLE();
//Variable setup
memset (&timer_cap_mdata_, 0x00, sizeof (timer_cap_mdata_));
timer_cap_ovf_callback_ = 0;After that, I setup one channel (at this case, channel 4, i.e. idx = 3) by calling function set_callback:
int set_callback (uint8_t idx, timer_cap_mode_t config, time_callback_t timer_callback){
//Previous check
if (!(idx < TIMER_CALLBACK_NMAX)) return -1;
//Callback refresh
timer_cap_mdata_[idx].isr = timer_callback;
//Starts callback overflow
timer_cap_mdata_[idx].ovfs = 0;
//If callback have assigned value, starts capture
if (timer_cap_mdata_[idx].isr)
{
//Setting up capture mode
configure_edge(idx, config);
//Starts interrupt
start_reference(idx);
}
else
{
//Stops interrupt
timer_cap_stop_reference(idx);
}
return 0;
}
static int configure_edge (uint32_t idx, timer_cap_mode_t config)
{
int channel;
GPIO_TypeDef *gport;
GPIO_InitTypeDef gstruct;
if ((channel = timer_cap_idx2channel(idx)) < 0)
{
return -1;
}
switch (idx)
{
case 0:
gport = GPIOA;
gstruct.Pin = GPIO_PIN_15;
break;
case 1:
gport = GPIOB;
gstruct.Pin = GPIO_PIN_3;
break;
case 2:
gport = GPIOB;
gstruct.Pin = GPIO_PIN_10;
break;
case 3:
gport = GPIOB;
gstruct.Pin = GPIO_PIN_11;
break;
default:
return -1;
}
//Setup PIN
gstruct.Mode = GPIO_MODE_INPUT;
gstruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(gport, &gstruct);
timer_cap_mdata_[idx].gport = *gport;
timer_cap_mdata_[idx].gpin = gstruct.Pin;
//Struct for input capture setup
TIM_IC_InitTypeDef sICConfig;
sICConfig.ICPolarity = 0;
sICConfig.ICSelection = TIM_ICSELECTION_DIRECTTI;
sICConfig.ICPrescaler = TIM_ICPSC_DIV1;
sICConfig.ICFilter = 0;
//Register the mode
timer_cap_mdata_[idx].gmode = config;
//Setup the edge
if (config == TIMER_CAP_RISING)
{
sICConfig.ICPolarity = TIM_ICPOLARITY_RISING;
}
else if (config == TIMER_CAP_FALLING)
{
sICConfig.ICPolarity = TIM_ICPOLARITY_FALLING;
}
else if (config == TIMER_CAP_BOTH)
{
GPIO_PinState valueP = HAL_GPIO_ReadPin (&timer_cap_mdata_[idx].gport, timer_cap_mdata_[idx].gpin);
if (valueP)
{
sICConfig.ICPolarity = TIM_ICPOLARITY_FALLING;
}
else
{
sICConfig.ICPolarity = TIM_ICPOLARITY_RISING;
}
}
//Setup channel
if(HAL_TIM_IC_ConfigChannel(&timer_cap_timhandle_, &sICConfig, channel) != HAL_OK)
{
return -1;
}
return 0;
}
static int start_reference (uint32_t idx)
{
//Timer2 enable interrupt
switch (idx){
case 0:
if(HAL_TIM_IC_Start_IT(&timer_cap_timhandle_, TIM_CHANNEL_1) != HAL_OK)
return -1;
break;
case 1:
if(HAL_TIM_IC_Start_IT(&timer_cap_timhandle_, TIM_CHANNEL_2) != HAL_OK)
return -1;
break;
case 2:
if(HAL_TIM_IC_Start_IT(&timer_cap_timhandle_, TIM_CHANNEL_3) != HAL_OK)
return -1;
break;
case 3:
if(HAL_TIM_IC_Start_IT(&timer_cap_timhandle_, TIM_CHANNEL_4) != HAL_OK)
return -1;
break;
default:
return -1;
}
return 0;
}Why I am not having any interrupt? My registers value after set_callback function is next:
Which seems to be OK. So, what's the matter? Why I'm not getting any interrupt?
I'm using STM32105VC microcontroller.
Thank you in advance!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.