STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 DAC with DMA constant value

Posted on April 12, 2018 at 20:07Hi to all,I am encountering a problem, concerning the DAC of the stm32L476. I only want to use the DAC with a constant value but with DMA, so that I can use the CPU during that operation. Without DMA the DAC works as...

Bench by Associate III
  • 5012 Views
  • 9 replies
  • 0 kudos

STM32H743XI HDMI connections

I am planning to implement STM32H743XI on my new design. And I am using the help of schematic provided for the eval board for the connection. I want to implement HDMI on my design too but the neither the schematic or the datasheet has the informatio...

BBV by Associate II
  • 3297 Views
  • 4 replies
  • 0 kudos

[How to] 5 Electrode Materials for Capacitive Touch Sensors (ITO,Metal Mesh,Silver Nanowires,Carbon Nanotubes,PEDOT:PSS)

Electrode behavior heavily depends on the material they are made off.To know if emerging materials can potentially be used as electrodes in touch sensors, we must first describe the properties we would want such a material to have.Desired properties ...

PAram by Associate II
  • 1587 Views
  • 0 replies
  • 0 kudos

STM32L0x1. RAM in low-power sleep mode.

STM32L0x1 reference manual says "the memory interface clock is stopped and the RAM is in power-down when in Low-power sleep mode" (DocID025942 Rev 8 p 145). Several pages below it says "In Low-power sleep mode, the Flash memory can be switched off an...

STM32H7 ADC QUEUE OF CONTEXT.

Hi,someone know a practical application of Injected queue of context for the STM32 ADC? I think that it would be more useful if the two JSQR values in the queue stay forever in the queue like a ring buffer.Asantos.

Asantos by Senior
  • 1055 Views
  • 0 replies
  • 0 kudos

SPI shift registers

Hello, In STM32F446RE mcu the block diagram shows 2 shift registers , but in STM32F407x spi block diagram it shows only shift diagram . which one is correct ? are these SPI IPs are different on these devices ? please clarify . i have attached the ima...

0690X000006DMsqQAG.png
n.serina by Associate III
  • 923 Views
  • 4 replies
  • 0 kudos

Hardware connection for uSD 4 Wire Bus

Hello,There is any schematic example for the connection between uSD and the STM32H7?I'm currently using a OLIMEX E407 with a STM32H7 instead of a STM32F4. It seems that I have problems with the signals integrity. I can read and write with a 1MHz cloc...

Damange92 by Associate II
  • 1026 Views
  • 1 replies
  • 0 kudos

STM32H750 KEIL

I USED KEIL WITH STM32F750VB AFTER COMPILE AND RUN I UNDRESTAND NO HAVE ANY SPACE ADD FOR STACK FIRST VARIABLE ADDRESS IS FIRST MEMORY ADDRESS IF USED PUSH OR PUP CHANGE SOME FIRST VARIABE IN MEMORY HOW CAN RESOLVED THIS PROBLEM

How to Choose the Most Flexible NUCLEO 'Range'?

We've been using a NUCLEO-L433RC-P to prototype a low -power PCB and it has served us very well.We're now embarking on a new project where we're actually going to use the NUCLEO and create a PCB with a header to plug the NUCLEO into. I thought this ...

MBrow.13 by Associate II
  • 1019 Views
  • 0 replies
  • 0 kudos

False LPTIM CMPM Interrupts ( STM32L071)

If the LPTIM CNT is close to the ARR value (0xFFFF) and i set the CMPM value, i receive the interrupt immediately (~1ms) instead of the time i set it. Because the LPTIM runs on 32kHz this happens every 2seconds for 4-5 interrupts.I dont seems to find...

DKilg by Associate II
  • 939 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.