STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using MSC to send data to GPIO PINS?

Can someone use MSC to send data to SPI or other GPIO Interfaces?I implemented a Project with Cube and now i want to test it by sending data through MSC to any GPIO or LED

arduo by Senior
  • 804 Views
  • 0 replies
  • 0 kudos

Resolved! Bug in MCU STM32L4 when trying to program the flash

I just run across a bug when trying to program the flash.You have to write two 32bit values for programming the flash. But if the first value is 0xFFFFFFFF it does not matter what the second value is. In the end there will always be written 0xFFFFFFF...

No I2C Clock signal after Restart Condition

Hello,I raised this problem in another topic I posted, but it is with another title and I'm not sure I will get there the help (title might be missleading).I have the problem after sending Slave Address and Register Address and creating a start condi...

0690X000006DUzQQAW.png
uli stone by Associate II
  • 5598 Views
  • 12 replies
  • 0 kudos

CAN on STM32F072C8

Dear ST sirs: We are using STM32F072C8, and we now have problem on its CAN bus. Like the below thread issue in the forum. However we did not see any reply on it.https://community.st.com/s/question/0D50X0000A4nF6FSQU/stm32f072c8-canbus-loopback-worki...

CHsu.14 by Associate II
  • 2517 Views
  • 3 replies
  • 0 kudos

Resolved! Time Triggered CAN communication support

I am currently in a process of selecting micro controller for my project. Basically i need TTCAN support and i have STM32F746G Disco board with me. Now as per the ST reference manual i see that this is supported. Now my questions are...Is there any ...

Resolved! Using lcd_log.c library function

Hi!!I'm using lcd_log.c to debug on the LCD.LCD_UsrLog ("This is Line% d \ n", i);Is there a way to change the starting position of text output?It always starts at the same location and scrolls down.Please, help me!!

DSEO by Associate II
  • 2327 Views
  • 3 replies
  • 0 kudos

spi adc

I am using stm32l476rg. I am connecting a external spi adc with 1.25MHz clock. I would like to have a continuous data reading from that adc. I tried spi2 to connect this adc. it works, but how can I get continuous data reading from that adc? use time...

yang hong by Associate III
  • 942 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.