2019-02-15 1:46 AM
Hello,
There is any schematic example for the connection between uSD and the STM32H7?
I'm currently using a OLIMEX E407 with a STM32H7 instead of a STM32F4. It seems that I have problems with the signals integrity. I can read and write with a 1MHz clock, if i go up with the frequency i can't write but i can read, like the problem is in the uSD side. If I increase the clock near the maximum possible, I can't even read.
Thanks in advantage,
Luca
2019-02-15 6:03 AM
Use similar length traces without stubs.
Use 33-47K pull ups on D0,D1,D2,D3, CMD, CARDDET at the SOCKET
Dial back the slew-rate, you don't need to push a 200 MHz edges down 2" of trace. ie SLOW or MEDIUM
Consider 33R series resistors if you're seeing ringing.
Turn OFF the use of the SD TRANSCEIVER in stm32h7xx_hal_conf,h
Have MicroSD cards simply attached to NUCLEO-H743ZI boards.
https://www.waveshare.com/micro-sd-storage-board.htm
https://www.waveshare.com/w/upload/8/83/Micro-SD-Storage-Board-Schematic.pdf
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.