STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

flash and CAN conflict?

Hello everybodyI was trying to store some data into flash and every time the erase page failed, the write completed if the memory was empty.I then found out that the erase is working until I send something over the CAN ( receive seems to not trip it)...

MA2 by Associate
  • 1462 Views
  • 1 replies
  • 0 kudos

Problem with USART communication between 2 processors

I have two STM32H743 processors which are connected by USART ports. We have to transmit data between these 2 µPs and have no other ports left (SPI or so) which could be used instead.I initialized the 2 USARTs using STM32CubeMX with the identical sett...

GS1 by Senior III
  • 2474 Views
  • 4 replies
  • 0 kudos

Programming STM32F730s from other STM32F730s

I need to program a large array of STM32F730s from a single master STM32F730. ST seems to have lots of applications notes on using bootloaders to pull code into these devices, and also on using STM-LInk to push code in. But what I need to do is pus...

MikeDB by Lead
  • 2985 Views
  • 10 replies
  • 0 kudos

SPI 1 line simplex rxonly

Hello, How to read data from slave in 1 line rxonly. I have this set up STM3f446re board as master and arduino uno as slaveMaster and slave are connected through only 2 lines. MISO and NSS. Master will be in rxonly mode and slave sends data to master...

n.serina by Associate III
  • 1404 Views
  • 3 replies
  • 0 kudos

wakeup from stop2 nucleo 144

Posted on June 23, 2018 at 12:13Hi,I'm trying to use the example code from cubeV.10           PWR-?PWR_STOP2_RTC.The only code I added was after the  SYSCLKConfig_STOP() function I added Init for LED 2 and turning it ON till the 5 sec delay then OFF...

STM32L010,in STOP mode 16 uA instead of <1uA

Hi,asking help for a behaviour that i was not able to find in previous discussions.i'm using for the first time this value line microcontroller :STM32L010K4T6 ,other production details printed on case are GQ20T VG CHN74815.I im using it on an empty P...

how booting from bank 2 stm of 32l475?

HelloI would like to boot my bank 1 or bank 2 card by activating / deactivating the BFB2.I created a program to flash an LED, I put the code in bank 1 at address 0x08000000 by flashing the LED at a certain frequency and then I put the same code but c...

Bfren.9 by Associate II
  • 2490 Views
  • 4 replies
  • 0 kudos

How create master/slave timer ?

Hello all,I work with the board stm32F746G discoI try to create a master/slave timer. I use the timer3 to master and timer2 in slave.I would like count every second with timer3 and for each trigger on timer3 i would like launch timer2 for a delay of ...

lidiriel by Associate II
  • 4617 Views
  • 6 replies
  • 1 kudos

Resolved! STM32L4 registers not being read during debugging

Hello,I am using an STM32L4R5VIT6 board in which I am programming it with Atollic TrueSTUDIO using the debugger and Jlink connectiong. When I am running the debugger, it suddenly stopped working for me and the console reads:Connecting to J-Link...  J...

BRoge by Associate II
  • 1145 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.