2019-02-15 6:20 AM
Hello,
How to read data from slave in 1 line rxonly.
I have this set up
STM3f446re board as master and arduino uno as slave
Master and slave are connected through only 2 lines. MISO and NSS.
Master will be in rxonly mode and slave sends data to master over MISO
Slave sends the data in the below format
<start byte><couple of bytes of data><end byte>
I can see master is continuously producing clock as expected .
But since master can sample at any clock edge i dont receive the data in order expected.
How to solve this issue?
Pls help
2019-02-15 8:51 AM
SPI is a synchronous bus with the master providing a clock signal. You might want to hook up the clock signal to the slave device.
2019-02-15 8:56 AM
If not confortable with SPI, start with 4 wires first. NSS, MISO, MOSI, SCK
2019-02-16 9:29 AM
You still can use normal duplex setup, and not bring out MOSI onto a pin in GPIO (unless you use a 'F1xx).
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.