STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! 32F769IDISCOVERY WiFi

I'm having a lot of trouble finding documentation. This board sold by ST exposes a connector that is intended to house an ESP8266 WiFi device. But the ST documentation says nothing about how that connector is wired on the board. I assume it's tied to...

Multiplexing with STM32F303

Hello ! I really need your help , im working on a project and its a game of luck , random numbers will appear on 4 x 7 Segments , so i must multiplex , i understood the principe but i can't reach some good results , i don't know why ...only the commo...

CHae by Associate
  • 1045 Views
  • 1 replies
  • 0 kudos

I2C Slave at STM32F401RE

Can anyone give me an example for an I2C-Slave at STM32F401RE?The delivered example I didnt understand...I can send Text from Mater to Slave Board, but then i dont know how to go further...I'm sitting hours at this...thanks,Christoph

CRich.1 by Associate
  • 772 Views
  • 0 replies
  • 0 kudos

External loader : SectorErase function is missing

Hello there!I'm trying to build an external loader for STM32H7, so I can use a NOR FLASH in XiP mode, but following the AN and the examples in CubeProgrammer folder, I'm getting the message:STM32CubeProgrammer API v1.4.0External loader : SectorErase ...

Peaga by Senior
  • 2600 Views
  • 6 replies
  • 0 kudos

USART with 7 data bits

Hi all!I am using STM32F427 with HAL. I have to communicate with other devices using communication protocol over RS-232 interface (USART). The protocol is using 7 data bits, odd parity. I am struggling to make it work. There is a setting for WordLeng...

Trouble Getting Peripherals to Work... At All

I have a custom board based on STM32H753. It has SDRAM, SD card slot, a couple of I2C peripherals, some GPIOs going to LEDs and a handful more that go to CPLDs which interface to another part of the system.I am not using generated HAL code or CubeMX ...

GSell by Associate
  • 1158 Views
  • 1 replies
  • 0 kudos

Programming arrays of STM32 MCUs

Still struggling with this so hopefully somebody can help me. As far as I can work out the STM32(H7s if it matters) need three pins (TCK, TMS & NRST) plus a common ground to be programmed from another MCU. I can't dedicate three pins on the master ...

MikeDB by Lead
  • 2339 Views
  • 9 replies
  • 0 kudos

STM32H750 in Europe

Are these parts US only?? I need 4 or 5 for prototyping.MOUSER: Will not ship outside USADIGIKEY: Will not ship outside USAST online: $70 postage to Europe. From USA. What else do you expect from a """European""" company.FARNEL : No not stock itRUTRO...

pr242 by Associate II
  • 4902 Views
  • 16 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.