STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Simple SPI Controller Behavior Question

Am I correct in thinking that an SPI controller in master mode connected to nothing else will send a clock burst whenever it is transmitting?I am troubleshooting an SPI application and it seems as if the master is never transmitting. When I scope SC...

PCROP becoming enabled

We ran a batch of boards with an STM32F401CE on them (this was not the first run of these boards or using this processor).After loading application code, about 10% of the boards became unresponsive. Looking into it we found in the option bytes on th...

BBrie by Associate II
  • 2930 Views
  • 6 replies
  • 0 kudos

STM32H750 SAI interfaces

It was suggested I look at this part as it's definitely superior to the F730. However I can't see how to use the SAI4 interface because its SCK_A and SCK_B pins are shared with those of SAI1. Am I missing something or does this preclude using both ...

MikeDB by Lead
  • 1699 Views
  • 2 replies
  • 0 kudos

Resolved! Reset line pulled low for no reason

I have created my own board based on the STM32L073RZ where I copied certain bits from the NUCLEO borad. I am having a problem where I can't connect to it using the STLINK. I have found out that even with only power plugged in the reset line is pulled...

Resolved! Why can't I change any value in the FLASH_OPTR register?

I am using the STM32L431 MCU and I want to stop the IWDG when it enters the standby mode, so I want to try changing the value of the IWDG_STDBY bit to freeze the IWDG. I tried with any of the the following instuctions but nothing works.CLEAR_BIT(FLAS...

BRuiz by Associate
  • 1116 Views
  • 1 replies
  • 0 kudos

如何知�?�STM32 �?�个型�?�的内部FLASH分布?

如何知�?�STM32 �?�个型�?�的内部FLASH分布?网上看到F10x微控制器的数�?�手册上有,但是上�?��?�有F101,F102,F102的,就连F100都没有,哪个数�?�手册�?�以看?知�?�的能�?能告诉我。�?�外关于F2,F3,F4,F7,L0,L1,L4 的数�?�手册也需�?,主�?是我需�?知�?��?�个型�?�的FLASH分布。类似下图

0690X000006Dlp6QAC.png 0690X000006DlpLQAS.png 0690X000006DlpGQAS.png 0690X000006DlpaQAC.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.