STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

F7 SDRAM CubeMX setup no DMA tab

The SDRAM HAL module has DMA functions but there is no tab in CubeMX to set up a mem2mem DMA channel. This is with CubemX 4.27.0. Is the DMA a pre-requisite for LTDC operation or does it use it's own internal memory access.

Temperature compensation on ADC?

Posted on August 11, 2017 at 05:02Hello, I am using an Olimex-E407 board to measure some signals (AC signals). After some reading on ADCs I learned that there are a few error that have to be taken into consideration when doing measurements and some ...

App fails when source is changed in a trivial way.

Hi,I've been playing around and refactoring a small test app for the STM32F769 DISCO board. The app runs fine and I retest after even the smallest code tweak.What I'm seeing is that physical position of the function SysTick_Handler within the source ...

0690X000006DoIyQAK.jpg 0690X000006DoJ8QAK.jpg 0690X000006DoJDQA0.jpg

Resolved! Understanding serial IO misbehavior

I've been trying to adapt an example piece of code that utilizes a UART from the Visual GDB website. The adaptations are:Using an STM32F769 Discovery board.Communicate with an ESP8266 device plugged into the board's WiFi socket.I managed to work out ...

0690X000006DoDeQAK.jpg

LTDC maximum display resolution documentation inconsistency?

Posted on January 10, 2018 at 02:34HiAN4861 (http://www.st.com/content/ccc/resource/technical/document/application_note/group0/25/ca/f9/b4/ae/fc/4e/1e/DM00287603/files/DM00287603.pdf/jcr:content/translations/en.DM00287603.pdf) page 25 states that th...

luke23 by Associate III
  • 2438 Views
  • 4 replies
  • 0 kudos

Sram to GPIO 8 bit transfer using DMA

Hello,I am a student of electrical engineering and I'm now starting a project where I need to use the stm32 architecture.The idea is to use a NUCLEO-H743ZI board and to connect 8bits of the GPIO to a VGA Cable and display a 640x480 60Hz 256 colors i...

JGon? by Associate
  • 1248 Views
  • 2 replies
  • 0 kudos

stm32l452, uart, when TXE = 1 ?

stm32l452, uart. CR1_TE is = 1, now I set CR1_TXEIE = 1. Is ISR-TXE = 1 (and INT generated) now too? Or really only if 'data is transferred to the shift register' ?

bso by Associate
  • 1581 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L4R9 GPIO13, 14, 15 EXTI interrupt problem

I think I've caused some problem in the way I'm coding this interrupt. For a second I thought it was a pipeline re-entry problem like Clive-Two-Zero described in a different thread, but adding a volatile variable and incrementing it, didn't seem to w...

Du1 by Senior
  • 2948 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.