STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CAN bus Network Problem

Hi everyone,I got a problem when i setup my can bus network. data 115200 Brate -> stm32f746vg(120 OHM //) --> CAN BUS----DEV1 --3M CABLE-- DEV2 --3M CABLE-- DEV3 (120 OHM //)    DEV1,2,3 = STM32F091CCI need to explain my installation. i have 4 device...

gunahmt by Associate II
  • 813 Views
  • 0 replies
  • 0 kudos

stm32f407 delay problem

Hi, I am using the stm32f407 card and I am developing keilda software but when I compile it does not fail but the delay does not work and I would be glad if you could help what could be the reason.

bnymntrz by Associate III
  • 1293 Views
  • 6 replies
  • 0 kudos

7 segment display and hc595

Do not use scanning method.Display with hc595 output.display doing blinkThe display does not remain steady when operating.I suspect Spi.I need helpthanks #include "stm32f4xx_conf.h"   #include "stm32f4xx.h"   #include <stdio.h>       #define CLK ...

kemal by Associate II
  • 2027 Views
  • 5 replies
  • 0 kudos

STM32F769I-DISC1 no speaker output via WM8994

Hi,I am currently developing with the STM32F769I-DISC1 development kit and get audio output via the CN7 Line Out connector when setting the initialisation to OUTPUT_DEVICE_HEADPHONE in the sample example as below: if(0 != audio_drv->Init(AUDIO_I2C_AD...

JFour.6 by Associate
  • 1248 Views
  • 1 replies
  • 1 kudos

Problem while receiving data from MEMS microphone.

I am using the STM32F407 discovery board and Wolfson pi audio interface. I have a problem in analysing sample values received from MEMS microphone.I wanted to plot the data sensed by the MEMS microphone, which is just sensing the surrounding environm...

rrach by Associate II
  • 1886 Views
  • 3 replies
  • 0 kudos

I2C by IT [solved]

Hi,I use I2C like this uint16_t I2cAddrTemp = 0x90; uint8_t I2cWritedata = 0x00; uint8_t I2cReaddata = 0xFF;   uint8_t read_i2c_temp(void) { hi2c1_status = HAL_I2C_Master_Transmit(&hi2c1, I2cAddrTemp, &I2cWritedata, 1, 1000); //PRINTF("I2c = %02X",...

MMath.10 by Associate II
  • 1268 Views
  • 0 replies
  • 0 kudos

Plug-in "com.st.microxplorer.rcp" was unable to instantiate class "com.st.microxplorer.eclipse.rcp.MicroXplorerView".

Hello, I've installed Eclipse IDE for C/C++ Dev (V. Oxygen.3a release 4.7.3a) in Windows 10.I've installed stm32 cube mx plugin (en.stsw-stm32095.zip) following procedure on UM1718 user manual ("Installing STM32CubeMX as an Eclipse IDE plug-in" parag...

LucaCMA by Associate II
  • 690 Views
  • 0 replies
  • 0 kudos

I2C2+DMA1 and UART4+DMA1

Hi all,I'm having some trouble getting DMA to service sequential uses of I2C+DMA transactions.​​​I can have the I2C+DMA initialize our demodulator, which involves some 12,000 reads and writes. (So, I2C+DMA works *very, very well* when it works.) I ca...

EJohn.17 by Associate II
  • 1944 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.