2018-09-11 10:16 AM
I'm working on a low power driver for our project and want to put the mcu into sleep mode to be woken up by a timer.
The mcu enters the Sleep mode but does not exit from the same. Since I have the Seggar J-link connected to over a JTAG port for debug, I can see that the RTC Alarm call back is being serviced and prints out the debugging information but the mcu does not exit the sleep mode.
Here is the code.
void PMODE_EnterSleep(void)
{
HAL_PWR_EnableSleepOnExit();
HAL_SuspendTick();
// Request to enter STOP PMODE with regulator in low power PMODE
HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFI);
}
void PMODE_ExitSleep(void)
{
HAL_PWR_DisableSleepOnExit();
SWD_PRINTF("Exiting Sleep\n");
}
// .... A general power mode servicing module
void PMODE_ServicePower(PMODE_eOperatingMode_t eModeToEnter)
{
switch (eModeToEnter)
{
case PMODE_eRun:
break;
case PMODE_eSleep:
SWD_PRINTF("Sleep\n");
PMODE_EnterSleep();
PMODE_ExitSleep();
break;
case PMODE_eStop:
SWD_PRINTF("Stop\n");
PMODE_EnterStop();
PMODE_ExitStop();
break;
case PMODE_eStandby:
SWD_PRINTF("Standby\n");
ALARM_ActivateWkup();
PMODE_EnterStandby();
break;
}
}Maybe I'm doing something wrong or not clearing a flag somewhere.
Further, I have several interrupts enabled in the applications main program, even those do not wake up the mcu.
I would appreciate any help.
Thank you.
Solved! Go to Solution.
2019-02-28 4:26 AM
Hello!
This answer is very late, but...
This line here:
HAL_PWR_EnableSleepOnExit();That function enables sleep on exit functionality, which means that your MCU will enter the sleep mode after exiting the lowest priority interrupt.
2019-02-28 4:26 AM
Hello!
This answer is very late, but...
This line here:
HAL_PWR_EnableSleepOnExit();That function enables sleep on exit functionality, which means that your MCU will enter the sleep mode after exiting the lowest priority interrupt.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.