STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407 SDIO/SDCard

Posted on March 29, 2018 at 04:32I am trying to get the STM407VET to communicate to an SD Card using the SDIO interface and drivers. Code base was generated from CubeMX and Eclipse is the IDE. Debugging with Open OCD. Hardware is custom. I have trac...

Resolved! FMC memory map confusion

Hello,I have a little confusion regarding FMC memory map. I hope someone can help me with it.Accoring to reference (stm32h743) FMC external memories are mapped as following:0x6C000000 -0x6FFFFFFF FMC NOR/PSRAM/SRAM 4 Bank1 (or remap of FMC SDRAM Ban...

ranran by Senior II
  • 4958 Views
  • 3 replies
  • 0 kudos

Hard fault caused by strncpy,

Hi,I am running into a strange problem, I am using strncpy function to copy one array into another. If i include this in my code i get a Hard fault DEBUG_VT . I have read quite few article on hard faults and how to track them down but this one that i...

conrad c by Associate II
  • 2742 Views
  • 3 replies
  • 0 kudos

Resolved! Help getting started with NUCLEO-F722ZE

So I've just bought a F722ZE based board which is ideal for the projects I'll be working on, however I was hoping I could get this to work with the arduino IDE and save myself the trouble of learning the new platform, but this doesn't seem to be poss...

JWood by Associate II
  • 2336 Views
  • 3 replies
  • 0 kudos

STM32L475RE only run in debug mode

Hi everyone!I’m working with a STM32L475RE design. The project works completely fine in “debug mode�? (using ULINK2) but doesn’t work in release mode. I’m trying to find the code part that could be the problem, using a LED on the initiation. However,...

STOP2 mode, voltage regulator, stm32cube

Posted on June 28, 2018 at 13:29Hi all,I'm trying low power modes of the STM32. I've noticed that HAL_PWREx_EnterSTOP2Mode synopsis mention that:  *        The voltage regulator is set in low-power mode but LPR bit must be cleared to enter stop 2 mo...

mh_stm by Associate II
  • 2011 Views
  • 2 replies
  • 0 kudos

Resolved! why the MCU stm32L011F3 has so small flash memory?

 the MCU stm32L011F3 has only 8k flash ,and without standard peripheral library, only HAL and LL library, as i know, the Optimization of HAL is lowest all of them, and LL driver is little Readiness,can any one tell me, is that the HAL driver can exec...

lming.0 by Associate II
  • 3325 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.