STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! stm32f103 14mhz adc clock and prescalers only allow 12mhz?

hi i'm reviewing rm0008 ref manual for stm32f103 the adc.accordingly, adc clock max is 14mhz and it takes 14 adc clock cycles for 1 conversion - hence 1msps per ADC.however, from the RCC section the available prescalers are 2, 4, 6, 8and if we take 7...

andrewg by Associate III
  • 2429 Views
  • 2 replies
  • 0 kudos

HardFault_Handler

Hi, I have a problem with HardFault_Handler.Sometimes, when I'm writing into the flash it happens.After many days on searching still I don't understand why it happens and what it means.Has someone got a suggestiom for me?

Expanding on ISRs generated by CubeMX

Dear AllCubeMX (Clive, I know you do not encourage relying on it, but please bear with me for a while) adds many c and h files to a project. Is the programmer allowed to modify any of such c files other than the main.c? For example, I see a void SyST...

Amir1 by Associate II
  • 849 Views
  • 0 replies
  • 0 kudos

ROS spinOnce jamming the process of MCU

We are using ROS Serial to let Raspberry Pi and STM32F103C8T6 communicate with each other. And there is another UART channel for IMU to use. We observe that the spinOnce function of ROS jammed the process of MCU. Therefore, other work cannot operate ...

STM32H7 series resistors in data lines ?

With a 400MHz clock and very high speed ports, I was assuming the faster data lines would need series resistors to avoid reflections in the way things like FPGAs do. But I've just noticed the evaluation board doesn't have any and routes even high spe...

MikeDB by Lead
  • 1477 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.