STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Multi channel ADC conversion with DMA and Interrupt.

hello everyone,i am new to STM32 controller series,i am trying to read mutli channel ADC with help of DMA and Interrupt.but facing issue.i am not getting ok status from"HAL_ADC_Start_DMA" this function. can any-body help me out.please find below con...

vshah by Associate II
  • 784 Views
  • 0 replies
  • 0 kudos

STM32H7 FMC setup for FT232H connection

I am trying to figure out how the FMC of an STM32H7 needs to be configured to work with an FT232H in CPU FIFO mode.The FT232H requires that for a write operation the NWE signal goes low after the data pins are set:From what I could find in the refere...

Alex A by Associate
  • 1871 Views
  • 1 replies
  • 0 kudos

Malloc to SD-Ram

I am using a STM32 Discovery Board with external SD Ram. I used the memory in RAM so far by creating a Ponter in the SD-Ram address area.But now my program is getting more and more complex and I could use a memory manager. Can I use the Malloc, Callo...

MMett by Associate III
  • 1777 Views
  • 2 replies
  • 0 kudos

STM32F4 USB hid host - non boot protocol

Posted on September 17, 2013 at 00:48 Dear All, Although this is my first post here, I am quite often reading my.st.com forum, when I need to find solution for my problems. Unfortunatley, this time I could not find the answer in existing threads for...

Resolved! Reference manual RM0360 got a mistake

Posted on October 29, 2015 at 11:54In the last version of RM0360,page 722, there is no description about the unique ID. But following the instruction of RM0091 I have read the 96bits ID out in some of my F030C8T6s .These numbers from several chips a...

Fail to detect STM32F103VC

Hi, this is first STM project and previously i do not have experience in st microelectronics controller but in other 32bit controller's.Our project based on following hardware and tools:STM32F103VCTST-Link V2 original toolsEclipse IDECube programming...

SB1 by Associate II
  • 816 Views
  • 0 replies
  • 0 kudos

A problem with STM STudio

When I want to import variables from the .elf file (generated by the TrueStudio, inside the Debug folder) into the STM Studio software, I get the below error. When I press OK and bypass it, it shows a list of variables, but none of them gets importe...

0690X0000060PqeQAE.jpg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.