STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STMFlashLoader Demo.exe on an STM32F756EVAL.

Trying to use the STMFlashLoader Demo.exe on an STM32F756EVAL. The auto baud detection in the UART bootloader seems to only sometimes work at 9600 baud. I try higher bauds but it fails. And there is no Speed command (0x03) like the CAN protocol has t...

rammit by Senior
  • 1736 Views
  • 3 replies
  • 0 kudos

Problems with BDMA (from memory to peripheral)

I need to do a project where I use the BDMA to transfer arrays from memory to the GPIO. The idea is to send the information in 8 bit parallel at 12.5MHz.I started with the DMA example from the STM32 (called DMAMUX_RequestGen) to try to understand how...

0690X0000088TNRQA2.png 0690X0000088TKcQAM.png 0690X0000088TLLQA2.jpg 0690X0000088TLpQAM.png
JGon? by Associate
  • 847 Views
  • 0 replies
  • 0 kudos

Resolved! Doubts about AN4013 and timer gated mode

Hello,an4013 Rev. 6 on page 21 writes:"The Counter Enable signal is generated by a logic OR between CEN control bit and the trigger input when configured in gated mode."while e.g. RM0351 writes:"Enable the counter by writing CEN=1 in the TIMx_CR1 reg...

WWDG Reset

I configured the WWDG using cubeMX and the init looks as follow: hwwdg.Instance = WWDG; hwwdg.Init.Prescaler = WWDG_PRESCALER_8; hwwdg.Init.Window = 127; hwwdg.Init.Counter = 127; hwwdg.Init.EWIMode = WWDG_EWI_ENABLE; if (HAL_WWDG_Init(&hw...

raffin by Associate III
  • 906 Views
  • 0 replies
  • 0 kudos

How to setup I2C

I am trying to connect the VL53L1X distance sensor to a B-L072z-lrwan dicoboard so it can send data using the lorawan stack .This is my first project using a hal and i cant get the I2C connection working.The output to my serial monitor is: 536872016...

TVoge by Associate II
  • 1518 Views
  • 1 replies
  • 0 kudos

Usart 1 how rs232

I need to use the serial usart1 how comunication and receiver data by interrupt​

FSant.18 by Associate II
  • 1409 Views
  • 3 replies
  • 0 kudos

where can I download ?

I read from "UM1727 User manual" The STM32 Nucleo examples, applications and demonstration are provided in one single .zip file. The extraction of the .zip file generates one folder, STM32 Nucleo_FW_VX.Y.Z, which contains the following subfolders. I...

szhiy.14 by Associate
  • 994 Views
  • 0 replies
  • 0 kudos

IDLE btween messages in USART

Hello,I want to seperate my TX messages with an IDLE frame (all 1) in order to be able the sync to it​ on the RX side by getting an IDLE interrupt.Is there an elegant way using the USART regs to verify that I send at least one IDLE before staring my ...

Yood by Associate II
  • 1157 Views
  • 1 replies
  • 0 kudos

Using 2 UART on STM32?

Dear Members,I want to read a result from my GPS,it's Neo 6MI initialized 2 UARTs UART 1 for PC and UART 2 for GPS,I got this result :INIT CODE GPS NEO - 6M....                           From GPS : Is it receiving properly ?The code : char in[8];pr...

0690X0000087jMhQAI.png
antonius by Senior
  • 10572 Views
  • 35 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.