STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How can I use my MPU5060 on STM32L432?

I found only a way to read MPU5060's values with STM32F :(I tried it on my STM32L but it seems that the suggested libraries are not compatible with STM32L.Can you help me please ?:)

abj by Associate
  • 703 Views
  • 0 replies
  • 0 kudos

Can running code find out the part number it's running on?

I'm writing code for STM32F042. If I'm running on the TSSOP20 package, I need to remap PA11 and PA12 to PA9 and PA10. For all other packages, I need to leave them alone.I can have a compile-time switch and generate different binaries for different pa...

AKrup by Associate II
  • 2340 Views
  • 4 replies
  • 0 kudos

Example of CAN RTR response message setup

I have the CAN functioning properly on the STM32F413 using Interrupts for Tx and Rx. I now want to add a response to an RTR message using the STM hardware only. I read the Ref Manual CAN chapter and the Datasheet. I understand how CAN functions and h...

KHule by Associate
  • 969 Views
  • 0 replies
  • 0 kudos

SMBUS with MLX90615 I am not able to get desired waveforms

I cant see a continuous clock. I want to put it in master mode and it seems to send only one byte and stops.Heres a snipetArray[0] = 0x27;   HAL_SMBUS_Master_Transmit_IT(&hsmbus3,0xB6, Array, 5, SMBUS_OTHER_FRAME_NO_PEC); while(HAL_SMBUS_GetState(&...

Resolved! How to test TIM1_CH3 for output of PWM ?

Hello everyone, I configured TIM1 for pwm. I will use CH3 and CH4. CH4 works well, but CH3 does not work. Sometimes when I load program first time CH3 works, But When I turn off the power and then turn on power CH3 does not work. Is there anyone who ...

Board: STM32F407G-DISC1, OS: ubuntu 16.04, IDE: Attolic TrueStudio, CubeMX(for code generation), Baud rate: 9600, Time Base Source : SysTick

Hi,I'm trying to receive data through USART2 through Arduino's serial terminal. I'm not able to receive anything. When I suspend the process, it is always stopping at UART_WaitOnFlagUntilTimeout(); . I'm using "HAL_UART_Receive(&huart2, rx_data, 10, ...

debug a CubeMx generated project

I want to debug a CubeMx Generated project on Nuelco-L496ZG board.In CubeMx, I created a project with only DCMI and related DMA, and generated the codes.Without adding any other code, I debugged the project in System Workbench for STM32,I thought the...

hsong.11 by Associate II
  • 863 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.