2025-04-17 7:42 PM
I am using STM32H747-DISCO board for development, and I try to access for MDIOs connectivity of the STM32H747, I found a document describe about MDIO:
STM32H7-Peripheral-Management data Input Output slave interface (MDIOS)
From the document it describes like the STM32H7 MDIO can go up to 16bits, can it go beyond that and modify it to read/write 32bit data?
If this model cannot support 32bit MDIO, does any other STM32 IC support 32bit MDIO?
2025-04-18 9:12 AM
Hi @Khey87
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Billy
2025-04-22 7:22 PM
Hi,
As discussed, there are two options of the ethernet setup.
1) STM32 MCU works as the slave (containing the ethernet PHY) and there is another master (containing the ethernet MAC) to control the STM32 MCU via the MDIO bus. From STM32 MCU point of view, it's MDIOS (MDIO slave) and what "STM32H7 - MDIOS" online doc covers.
2) STM32 MCU works as the master (MAC) which connects with another slave device (PHY) via MDIO. This MDIO is part of the ethernet interface.
The customer confirms that their setup is the 2nd one. STM32H747 supports MDIO (Clause 22 and Clause 45) master interface for PHY device configuration and management.
Best Regards,
Feng
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.