STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Adding LED APIs for STM32L476 Discovery board?

I am trying to create keil project for STM32L476VG Discovery board, I tried to include LED API through board support packages from Manage Run time environment.It leads to open STM32CubeMx and I have generated the code, While building the code I am ge...

SSaur by Associate II
  • 1660 Views
  • 3 replies
  • 0 kudos

Running STMCUFINDER in 64-bit Linux (Opensuse)

Hello,recent STMCUFINDER installs without errors on Opensuse Leqp-15.0. Running as in the 32 or 64 bit ennvironment however gives: LANG=C linux32 ./STMCUFinderchdir /devel/STMCUFinder/.current dir /devel/STMCUFinderError: Unable to initialize main cl...

Run code from external RAM

Hello,for a new project I plan to execute the code from an external SRAM connected via FMC.Are there any experience on speed leakage?In an other Topic I read that there are losses of 4 times the speed compared to the embedded Flash.https://community....

Bombadil by Associate II
  • 2396 Views
  • 3 replies
  • 0 kudos

resetting the WWDG

Hey everyone,I'm a little confused. I've added the wwdg, but I'm not sure where to refresh it. Is there somewhere I can refresh it that should happen at a constant time, The examples I looked at simply place the reset in the code, but I have so many ...

con3 by Senior
  • 1660 Views
  • 2 replies
  • 0 kudos

Resolved! NUCLEO-F722ZE I2C2 in slave mode doesn't work nothing.

Hi,I am using NUCLEO -F722ZE board for testing the STM32F7 and their peripheral features. Other peripherals I tested works fine, but I have encountered a problem with I2C2 in slave mode, that doesn't send ACK when the master calls it (status flags ke...

0690X0000088scvQAA.bmp
RCata by Associate III
  • 894 Views
  • 1 replies
  • 0 kudos

GPIO Speed

Hello everybody,I have to generate a pulse with very narrow and different widths. The setting and procedure is as follows: Clock Freq = 16 Mhz, Prescaler = 1. off time should be 15 μs,  thuss = 15 μs * 16MHz / 2 = 120  Counts and with this logic for ...

Samuel1 by Associate III
  • 1912 Views
  • 3 replies
  • 0 kudos

Why placing breakpoints after enabling and starting USART DMA transfer in STM32F429I Discovery board corrupts my program execution?

Hi EveryoneI am working on a FreeRTOS based application in which I have to enable USART DMA channel to transmit 16 bytes of buffer from memory to USART Data Register in a task. It happens every time my task is invoked. Everything seems to work fine u...

MSaif by Associate II
  • 1624 Views
  • 2 replies
  • 0 kudos

multi master spi

Hey everyone,I've been struggling with the multi-master spi. I can send and receive seperately but when I try to integrate it into one program it bogs out. My understanding is that I can set the SPI line as a slave and then whenever I want it to act ...

con3 by Senior
  • 3359 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.