2018-11-09 2:22 AM
Hello,
recent STMCUFINDER installs without errors on Opensuse Leqp-15.0. Running as in the 32 or 64 bit ennvironment however gives:
LANG=C linux32 ./STMCUFinder
chdir /devel/STMCUFinder/.
current dir /devel/STMCUFinder
Error: Unable to initialize main class com.st.microxplorer.mcufinder.StandaloneMcuFinder
Caused by: java.lang.NoClassDefFoundError: com/sun/java/swing/plaf/windows/WindowsLookAndFeel
bon@hertz:~/devel/STMCUFinder> LANG=C ./STMCUFinder
chdir /devel/STMCUFinder/.
current dir /devel/STMCUFinder
Error: Unable to initialize main class com.st.microxplorer.mcufinder.StandaloneMcuFinder
Caused by: java.lang.NoClassDefFoundError: com/sun/java/swing/plaf/windows/WindowsLookAndFeel
I tried many combinations, including download and stlall of Orace jre and switching to that alternative, with no different error:
# update-alternatives --config java
There are 3 choices for the alternative java (providing /usr/bin/java).
Selection Path Priority Status
------------------------------------------------------------
0 /usr/lib64/jvm/jre-10-openjdk/bin/java 2005 auto mode
1 /usr/java/latest/bin/java 1 manual mode
* 2 /usr/lib64/jvm/jre-1.8.0-openjdk/bin/java 1805 manual mode
3 /usr/lib64/jvm/jre-10-openjdk/bin/java 2005 manual mode
Any ideas what to do?
Thanks
2018-11-09 2:45 AM
Hello Uwe,
I will escalate this issue to our MCU finder experts, and one of them will come back to you later to provide more help.
I wonder if the same issue is faced with STM32CubeMX (which embeds an MCU Finder) or not?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-11-09 3:17 AM
Installing Cube goes fine and starting a new project starts the STMCUFINDER fine Is there a way to start STMCUFINDER direct from the STM32CubeMX directory without first starting CUBEMX?
2019-03-26 8:55 AM
will be fixed in a next release
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.