STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F77* SDRAM FMC, Can you pin swap data and address pins?

I am wondering if you can pin swap the data pins ( withing byte lanes) without any software consequences? If their are any is it easy to resolve?I am also wondering if you can pin swap the address pins at all and if you do can you do it without any s...

TallGUY by Associate II
  • 2025 Views
  • 3 replies
  • 0 kudos

Resolved! Get statt with STM32F103C8T6

I am working on project in which we are using STM32F103C8T6 and I have one development board called blue pill and also have st link V2.But I don’t know where to start which are the softwares are required for STM32 development. I have searched on the ...

JPanc.1 by Associate II
  • 1316 Views
  • 2 replies
  • 0 kudos

STM32F030CC 48MHz PLL and SysTick...What am I missing?

Hi,I'm trying to set the PLL output to 48MHz on a STM32F030CC:HSI = 8MHzRCC->CFGR PLLSRC = 0 (PLL input = HSI/2), PREDIV = not divided.PLLMUL = 12;should give (8MHz/2) * 12 = 48MHz but instead I get no clock output on MCO.Using the MCO output I have ...

Tim_24 by Associate II
  • 1747 Views
  • 3 replies
  • 0 kudos

L433 UART Tx Output is Not What is Being Sent

Hello:I am trying to determine why the LPUART is transmitting out the values I am seeing. They make little sense. Here is the UART setup:void MX_LPUART1_UART_Init(void){ hlpuart1.Instance = LPUART1; hlpuart1.Init.BaudRate = 9600; hlpuart1.Init.WordLe...

ITM_SendChar on NUCLEO-F767ZI with ST-Link Utility

Hi,I've got a NUCLEO-F767ZI and I've just tried calling ITM_SendChar and watching for the output using ST-Link Utility SWO Viewer.I see some strange characters in the SWO Viewer but not what I've sent.It looks like it is sort of working but that the ...

MBrow.13 by Associate II
  • 1270 Views
  • 1 replies
  • 0 kudos

SQLite on STM32F7 series

I'm trying to implement a DataBase connection with STM32F779NIHx. I included the sqlite sources but received an error because the ioctl.h file is not present within the STM32F7XX HAL Driver. Where can I retrieve it?

GPapa.7 by Associate
  • 2264 Views
  • 3 replies
  • 0 kudos

Cycle Counter different when stepping

Hello,I'm currently doing some performance measurements using the DWT's CYCCNT register. As I understand the RM, the CYCCNT counts up for every core clock cycle (except when halted). However, I get different values in CYCCNT when stepping through the...

TLudw by Associate II
  • 2767 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.