2019-03-27 4:21 AM
I save config data (40 bytes total) in a dedicated flash sector (in my case sector 3)
with the application running on the board. Before I write the sector is erased.
I write several words with multiple calls of HAL_FLASH_Program(FLASH_TYPEPROGRAM_HALFWORD, adr, word);
Every data byte is written correct except at position 2 and 3.
Byte number 2 and 3 are 0x00 all the time.
There is no error returned.
Unfortunately the device is at a customer, working in production.
But I'm able to write new firmware via Ethernet IAP to do some tests.
Does anyone have the same issue data written is not the same as read?
Thank you
Joerg
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.