2019-03-27 12:43 PM
Hello:
I seemingly have the LPUART now configured correctly. For sure the transmit (without DMA) functions OK. I only have receive DMA configured. As usual, it was done in Cube.
uint8_t rxBuff[40];
#define RX_DMA_SZ 10
The start is the same as I am using in another program that does work:
HAL_UART_Receive_DMA(&hlpuart1, (uint8_t*)rxBuff, RX_DMA_SZ);
I also have both half/complete callback defined.
When Teraterm sends characters I can see them on the receive line from the 485 transceiver to the L433. I have a breakpoint in the interrupt under the IRQ interrupt and the DMA interrupt. The breakpoint is never hit.
I have an ADC DMA that works just fine, this one doesn't feel quite the same. What would cause the UART DMA not to function?
Solved! Go to Solution.
2019-03-27 2:02 PM
Found issue. Had the LPUART global interrupt still enabled.
2019-03-27 1:38 PM
Hi,
I removed everything from the CubeMX configurator with the exception of 5 pins:
LPUART RX
LPUART TX
UART TX CONTROL (GPIO)
SWDIO
SWCLK
Regenerated the code. Put a breakpoint on:
HAL_DMA_IRQHandler(&hdma_lpuart_rx);
and on:
HAL_UART_IRQHandler(&hlpuart1);
Neither gets hit.
I scope the RX line and see good data going into to abyss, but the device does not respond.
What in the world is going on? Can anyone offer a suggestion?
2019-03-27 1:59 PM
Polled Rx works?
JW
2019-03-27 2:02 PM
Found issue. Had the LPUART global interrupt still enabled.
2019-03-27 3:11 PM
silly oversight. I did not catch the IRQ was also enabled. I suppose the software gets a bit confused? Thanks for looking at this post.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.