STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

about gpdma transmission size

I am porting code from G473 to U575 because I need more flash and ram.Then I meet some issues on gpdma transmission size.For G473, I use dma to transfer data to timer ARR likes:uint16_t buf[65536] = { ..... };HAL_TIM_Base_Start_DMA(&htim1, (uint32_t ...

dh_leslie by Associate II
  • 2898 Views
  • 9 replies
  • 0 kudos

Generating PWM TIM8 STM32F4 initialization

Hello community, I want to generate PWM with tim8 CH1 and CH1N (complementary) but i have an issue. CH1 pwm first pulse is 2x what it must be. My APB2 clock is 84MHz and i am generating an 500kHz PWM. How to initialize well the PWM with tim 8 to have...

Didinano_0-1745504022718.png Didinano_0-1745511732352.jpeg Didinano_1-1745504080588.png
Didinano by Associate II
  • 1640 Views
  • 3 replies
  • 3 kudos

U5 DSI Communications Issues

This is a repost of the message I left on the "STM32 MCUs Touch GFX and GUI" and I'm hoping that it gets some more traction in this section of the forum.Apologies for the repost. I'm in the process of migrating from an STM32F779AIY6TR to an STM32U5A9...

STM32H753VIH6_Leakage Current data

Hi Team,We used the STM32H753VIH6 in our current design and validatedWe are looking for the leakage current data of the STM32H753VIH6.We want to validate the leakage consumption under no load condition.Please provide the data on this.  Regards,Sathya...

Serial decoder 4b5b

Hello Dear Community,I want to capture and decode a bitstream on STM32F746. The bit rate is 60ns/bit. Data is encoded using 4b5b and has a unique code for start of frame and no end of frame.What I have tried so far, is to configure TIM2 (APB1 timer c...

Lowest pin count QFP STM32 LCD RGB FMC

Hi ST community,I am looking for some help with selecting the lowest QFP pin count STM32 for my project.The STM32 will connect to the following below:18/24bit RGB LCDFMCQSPImaybe MIPI (Optional)Any FMC part number suggestion?Thanks

Gen-Tune by Associate II
  • 1031 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.