STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LED blinks only in debug mode

Hi!I have a basic code - blinking LED code which uses onboard LED (PC13). The problem is that it doesn't toggle at all, it just stay switched on and doesn't go off after delay. I've tested that code in debug mode and everything worked fine, it toggl...

astaria by Associate II
  • 2766 Views
  • 3 replies
  • 0 kudos

How to speed up IRQ times at STM32F7xxx ?

CPU 210MHzIf you run IRQ code from flash you have about 5 times more cpu cycles as needed (7WS)if you switch on ART accelerater and prefetch: for loop gets slower no influence on IRQ latencyyou could not run code from internal SRAM because of missin...

BSchm.0 by Associate II
  • 2237 Views
  • 3 replies
  • 0 kudos

STM32F767ZI could not remapped to internal SRAM

Hi folks, I have tried to run my complete program out of internal SRAM to speed up the IRQsbut if I come to svc 0 it failsprvPortStartFirstTask: 20005ee0: ldr r0, [pc, #32] ; (0x20005f04) 20005ee2: ldr r0, [r0, #0] 20005ee4: ldr r...

0690X000008a8P8QAI.png
BSchm.0 by Associate II
  • 1355 Views
  • 1 replies
  • 0 kudos

STM32F765IIK6 Reflow Problems

We are using STM32F765IIK6 176 pin 10x10 0.6mm UFBGA, die rev "Z". Whilst processing these through SMT solder reflow (using an 8 zone forced air convection oven) we had a number of these devices failing, due to the substrate of the BGA package dishin...

MBake by Associate
  • 1290 Views
  • 1 replies
  • 0 kudos

production ready STM32 boards

Hi,Does anyone know if there are any companies out there that sell production ready stm32 hardware boards. I appreciated there would be a lot of variations regarding io etc.. but i just wondered if it was a "thing" or if the only board are typically ...

Resolved! STM32L431 can't enter STOP2 mode

I'm trying to enter STOP2 mode to save energy but the MCU get stuck in the function HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI). I have cleared all EXTI pending flags and RTC flags, and disable all five wake up pins. The MCU is supposed to wake up vi...

TClar.8 by Associate II
  • 7583 Views
  • 11 replies
  • 0 kudos

Resolved! STM32 General Purpose Timer Update Event and glitch problem

I use STM32F102 and TIM2 timer in PWM1 mode to generate defined frequency and duty cyclesquare wave. I have some questions and I hope can get some help from experienced colleagues.1. I update the ARR/CCR1 register in an interrput which is defined by ...

NCTUser by Associate III
  • 6378 Views
  • 5 replies
  • 0 kudos

I am working on STM32H743 micro operating as a slave I2C device. I am able to write to the slave device by a master I2C device but I can't seem to read.

I have done some investigation and arrived that the problem is with the "DIR" bit in the Interrupt Status register not firing to indicate whether to do a Read.uint32_t isr_trace[64]; int isr_count = 0;   void I2C2_EV_IRQHandler(void) { isr_trace[...

onio by Senior
  • 2083 Views
  • 5 replies
  • 0 kudos

[How to] From Mechanical to Capacitive controls Guide (Buttons with sharp edges and 2mm clearance, 2 layer pcb with cover glass (50x70mm))

Even though most of you may be relatively familiar with the various types of mechanical controls, the same does not necessarily apply for capacitive ones. So, let’s start off by defining the most basic elements of capacitive sensing.Capacitive button...

PAram by Associate II
  • 1686 Views
  • 0 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.