STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

how to find I2C address for MX_I2C1_Init()

I am using nucleo L476RG with ​DS2482-100, also 1-wire DS28EC20 is connected with DS2482-100.  First I created the project with CubeMX, then  MX_I2C1_Init() My first question is: how to find the I2C address, which I need to fill hi2c1.Init.OwnAddress...

adam.wu by Associate II
  • 1013 Views
  • 0 replies
  • 0 kudos

Have I run out of Memory, RAM Overflow

Hi,I'm having trouble, because I got when I defined a second array which I need for processing a image with the STM32F429ZI Microcontroller a message that I have a RAM overflow.When I now define a smaller array, like uint8_t image[240][320] my whole ...

uli stone by Associate II
  • 14528 Views
  • 21 replies
  • 0 kudos

STM32L073RZ GPIO EXTI Interrupt not triggering callback

I'm working with an STM32L073RZ on a custom board. The board is in STOP mode and I have a pin (PB_5) configured as a rising edge interrupt. I'm using ARM Mbed OS 5.12.0 but primarily working with the HAL API. The code I have so far is below. It simpl...

Fatal Error[Pe035]: #error directive: "Please select first the target STM32F10x device used in your application (in stm32f10x.h file)" C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.3\arm\CMSIS\DSP\Include\stm32f10x.h 96

Hi I am trying to write a code using STM32f103r8t6, i have installed IAR for Arm v8.40.1 i started to create a project but i could not find any library files. and then by downloading an example file i got the library files as i tried to complile i m ...

Skuma.18 by Associate II
  • 5189 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.