2019-05-27 2:17 PM
Hi!
I have a basic code - blinking LED code which uses onboard LED (PC13). The problem is that it doesn't toggle at all, it just stay switched on and doesn't go off after delay. I've tested that code in debug mode and everything worked fine, it toggled, but it doesn't work out of debug. I can't get why it works only during debugging and how to fix that.
Board - STM32F103C8T6
Utility is STM32 ST-LINK Utility v4.4.0
Driver is STSW-LINK009
Programmer st-link v2
Code:
------------------------------------------------------------------------------------------
#include "stm32f10x.h"
#include "stm32f10x_rcc.h"
#include "stm32f10x_gpio.h"
GPIO_InitTypeDef GPIO_InitStruct;
void delay(int a);
int main(void)
{
// Enable clock for GPIOC
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE);
// Configure PC13
GPIO_InitStruct.GPIO_Pin = GPIO_Pin_13;
GPIO_InitStruct.GPIO_Speed = GPIO_Speed_2MHz;
GPIO_InitStruct.GPIO_Mode = GPIO_Mode_Out_PP;
GPIO_Init(GPIOC, &GPIO_InitStruct);
while (1)
{
// Turn on LED on PC13
GPIO_ResetBits(GPIOC, GPIO_Pin_13);
delay(5000);
// Turn off LED on PC13
GPIO_SetBits(GPIOC, GPIO_Pin_13);
delay(5000);
}
}
void delay (int a)
{
volatile int i,j;
for (i=0 ; i < a ; i++)
{
j++;
}
return;
}
----------------------------------------------------------------------------------------------------
Waiting for your advice a lot ;)
Solved! Go to Solution.
2019-05-27 9:26 PM
72 MHz means about 14 ns per clock tick. The processor executes most instructions in 1 clock cycle.
The compiler probably optimizes that loop to roughly 3 or 4 instructions.
that means about 55 ns per loop. So 5000 loops should take roughly 300 us.
You should not see it blink, but you should see it glow.
2019-05-27 3:31 PM
At several million cycles, 5000 ain't much. Push out the number, and perhaps scope so you can see a square wave.
Perhaps use SysTick.
2019-05-27 9:26 PM
72 MHz means about 14 ns per clock tick. The processor executes most instructions in 1 clock cycle.
The compiler probably optimizes that loop to roughly 3 or 4 instructions.
that means about 55 ns per loop. So 5000 loops should take roughly 300 us.
You should not see it blink, but you should see it glow.
2019-05-29 9:55 AM
yeah, i've set it up to 5000000 and it finally started to be noticeable. Thank you!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.