STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

using 32 MHz crystall with STM32L011K4

Hi,In a project I need a precise timing so I cant rely on th internal oscilator and want to use a crystal 24-32MHz with MCU. But actually I couldnt find anything about this possibility in datasheet.the sample is 32 KHz that is not good for my applica...

MKora by Associate II
  • 1764 Views
  • 4 replies
  • 0 kudos

Why Linker file needs to be modified to use External memory(RAM/Flash) if I can access external memory using communication modes like SPI,I2C,etc ?

I have seen many examples to use external memory as heap but for it they have modified the linker and added section of needed memory. But I am curious if I can access the external memory using standard communication interfaces like I2c, SPI, etc then...

Mrunal A by Associate III
  • 1613 Views
  • 2 replies
  • 1 kudos

L4 color space clut

I only need to display around 8 colors in rgb space and if i use L4 color space i can reduce my framebuffer to the point where i can put the entire framebuffer in internal sram. The only problem is i don't understand how to format the clut in L4.

Badam.17 by Associate II
  • 1331 Views
  • 1 replies
  • 0 kudos

Under what conditions does bxCAN fail to transmit?

Hello, I am working on a project trying to merge 2 discrete CAN buses with the STM32F746zgt6 using bxCAN with the HAL drivers. This system will take packets in on both transceivers, one on each bus, and try to output on the opposite transceiver, esse...

ARigg by Associate
  • 693 Views
  • 0 replies
  • 0 kudos

STM32F415 - Automatic Erase of Flash on power ON

I am using Mini-M4 module with STMF415RG MCU. Module is programmed using STLink SW interface. However when the module is put on to the mother board, the flash memory gets erased when the board is powered on. What can be the reason for this automati...

MJain.7 by Associate
  • 1557 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.