2018-10-12 6:00 AM
2018-10-12 6:05 AM
Hi. In order to take the uuid from a stm32f091 microcontroller I'm using these lines of code:
#define UUID0 ((uint32_t *)0x1ffff7ac)
#define UUID1 ((uint32_t *)0x1ffff7b0)
#define UUID2 ((uint32_t *)0x1ffff7b4)
std::vector<unsigned char> UUID_Vector;
UUID_Vector.push_back(UUID0[3]);
UUID_Vector.push_back(UUID0[2]);
UUID_Vector.push_back(UUID0[1]);
UUID_Vector.push_back(UUID0[0]);
UUID_Vector.push_back(UUID1[3]);
UUID_Vector.push_back(UUID1[2]);
UUID_Vector.push_back(UUID1[1]);
UUID_Vector.push_back(UUID1[0]);
UUID_Vector.push_back(UUID2[3]);
UUID_Vector.push_back(UUID2[2]);
UUID_Vector.push_back(UUID2[1]);
UUID_Vector.push_back(UUID2[0]);There UUID0[3] is the less significative byte and UUID2[0] is the most significative byte.
Is thi right?
2019-06-25 7:20 AM
I have written the code above according with these articles:
https://techoverflow.net/2015/02/03/reading-the-stm32-unique-device-id-in-c/
https://gist.github.com/ElectronicaXAB3/2e1085be2719990f178d0557dc8314d1
http://blog.gorski.pm/stm32-unique-id
But after having installed 50 devices based on a stm32f091 micro controller the uuid is not unique, I have found 4 duplicate uuids.
So where is the error in the code?
2019-06-25 8:33 AM
I think it should be #define UUID0 ((uint8_t *)0x1ffff7ac).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.