2019-06-10 9:48 PM
I'm configuring RTC AlarmA to wake up CPU from StandBy. I'am expecting to CPU became back at specified time, but it event occurs up to 16 seconds later.
uint32_t time;
uint32_t date;
uint32_t subsec;
do {
time = LL_RTC_TIME_Get(RTC);
date = LL_RTC_DATE_Get(RTC);
subsec = LL_RTC_TIME_GetSubSecond(RTC);
} while (subsec != LL_RTC_TIME_GetSubSecond(RTC));
sec = __LL_RTC_CONVERT_BCD2BIN(__LL_RTC_GET_SECOND(time));
min = __LL_RTC_CONVERT_BCD2BIN(__LL_RTC_GET_MINUTE(time));
hour= __LL_RTC_CONVERT_BCD2BIN(__LL_RTC_GET_HOUR(time));
sec+=10; //
LL_RTC_DisableWriteProtection(RTC);
CLEAR_BIT(PWR->CSR, PWR_CSR_EWUP);
LL_RTC_ALMA_Disable(RTC);
do {} while (!LL_RTC_IsActiveFlag_ALRAW(RTC));
LL_RTC_ClearFlag_ALRA(RTC);
LL_RTC_ALMA_ConfigTime(RTC, LL_RTC_ALMA_TIME_FORMAT_AM, __LL_RTC_CONVERT_BIN2BCD(hour), __LL_RTC_CONVERT_BIN2BCD(min), __LL_RTC_CONVERT_BIN2BCD(sec));
LL_RTC_ALMA_SetMask(RTC, LL_RTC_ALMA_MASK_DATEWEEKDAY | LL_RTC_ALMA_MASK_HOURS | LL_RTC_ALMA_MASK_MINUTES);
LL_RTC_ALMA_SetSubSecondMask(RTC, 0);
LL_RTC_ALMA_Enable(RTC);
LL_RTC_EnableWriteProtection(RTC);
TRACE_INFO("RTC->ALRMAR: 0x%08X\r\n",RTC->ALRMAR);
/* Enable the wake up pin */
SET_BIT(PWR->CSR, PWR_CSR_EWUP);
SET_BIT(PWR->CR, PWR_CR_PDDS | PWR_CR_CWUF | PWR_CR_CSBF);
SET_BIT(SCB->SCR, ((uint32_t)SCB_SCR_SLEEPDEEP_Msk));
__WFI();If set time to WakeUp for example 00:00:10 -> CPU will WakeUp at 00:00:26 and so on. Always up to 16 seconds later.
What I do wrong?
2019-06-25 3:57 AM
Hello,
How you configure the RTC alarm ?
Try to use HAL library function.
Best Regards,
Mohamed Aymen.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.