STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F30f4, standard cube configured out of the box software locks up after fixed number of processor cycles. IO looks to resets also. Loops in system memory starting at 0x1ffffed68. Only if sysTick is enabled. Does not get to sysTick interrupt.

STM32F30f4 Does this in debug mode or release with and without STLINK attached via SWCLK Pin 20,SWDIO Pin 19,NRST Pin 4.Using HSI clock and PLL , but tried also without PLL. I've only enabled IO on the standard IO lines available, PA0 -> PA7 Pin 6 to...

PKnel by Associate II
  • 2362 Views
  • 4 replies
  • 0 kudos

Resolved! STM32H743 BDMA channel for SAI4 not described in Manual

I am trying to program BDMA of STM32H743 using Nucleo board to perform DMA Peripheral to Memory operation . What I have found a bit difficult is that I could not see any information on Reference Manual , Datasheet or on forum for the mapping informa...

A Maq by Senior
  • 1441 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F407 DISCOVERY board CAN example

I have tried to get the CAN peripheral up and running on STM32F407 discovery board.But I am stuck at one point. Inside method HAL_CAN_Init(CAN_HandleTypeDef *hcan), I end up in the HAL_CAN_STATE_ERROR.Is there any example available to test on the dis...

gowtham K by Associate II
  • 1605 Views
  • 2 replies
  • 0 kudos

FIT value of STM32

Hello,I need to know the FIT value of STM32F7 Series (STM32F746VGT,etc) to compute the reliability data.Could anyone tell me that information ?Thank you in advance.Toshiya

User.57 by Associate
  • 899 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.