2019-08-07 3:46 AM
Hi!
I have STM32F051K4Tx mcu. I would like to generate a short pulse of different width at each comparator event without using interrupt. Is this possible? How would I setup timer / comparator for this to work?
Thanks.
2019-08-07 4:35 AM
The answer to this question depends on the answer to this question.
If red, it's easy-peasy, just set it up as with triggering pulse with any external trigger.
If blue, which I suspect is more likely, then, well, it has to be changed so it's like red, and I suspect the easiest way to do that is to output the comparator's output to a pin and externally connect to the timer's input pin. There might be an alternative way using TRGO-TRGI to a linked timer and then generate the pulse there.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.