2019-08-07 2:23 AM
Hi
Earlier I was facing the problem to start the SAI communication when merging with BLE application.
Referred application
STM32CubeFunctionPack_BVLINK1_V1.0.0
Hardware
STM32L476RG nucleo 64
X-NUCLEO-IDB05A1
Update in the development.
Using same application code I am able to initialize SAI peripheral and it is receiving data using the function mentioned below,
if(HAL_SAI_Receive_DMA(&hsai_BlockB2,(uint8_t*)PCM_Buffer,16)!= HAL_OK)
{
return AUDIO_ERROR;
}
But now the problem is the device fails to stream data over BLE using Bluevoice service.
Devices not getting status BV_ADPCM_STATUS_STREAMING
Due to this it fails to stream the data. This library is not accessible so I am not able to find the reason for this.
Looking for help to get the solution.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.