STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

In stm32h7 issue with SDMMC speed

Actually i generated code for EMMC in cubeMX. I can able to write data with 1MBps. But i need 50MBps for this what can i change in driver file. i am using 8-Bit datamode.i tried with increase the clock frequency also the speed has not increased. Any ...

srikanth by Associate III
  • 1829 Views
  • 4 replies
  • 0 kudos

SPI1 DMA INTERRUPT AFTER EACH BYTE TRANSMISSION

Hello GuysThe IC I am communicating with via my Nucleo STM32F446 board uses SPI and require a Chip Select Low before each SPI byte transmitted, then CHIP SELECT high for x time and then low again for next byte.So I am using SPI via DMA which is desig...

JHERI by Senior
  • 2050 Views
  • 6 replies
  • 0 kudos

NSS pin has no effect on slave STM32F303 nucleo

Hello,I have two STM32F303RE nucleo boards one acting as a master and the other as a slave.I have flashed the SPI examples on both of them that come with the firmware and both master/slave are working properly.The issue is the example only uses (SCK,...

salman by Associate II
  • 2248 Views
  • 4 replies
  • 0 kudos

Resolved! How many 1.2V internal regulators on-chip for STM32F779NI ?

Hello,Micro-controller used : STM32F779NIQuestion:My understanding is that there are two 1.2 V internal regulators.[1] The regulator that gets enabled by holding BYPASS_REG pin as low[2] The backup regulator that gets enabled through PWR_CSR1.BREAm i...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.