2019-09-22 10:06 AM
2019-09-22 10:37 AM
They won't run properly at 180 MHz
The TIM nominally run at APB x2
Why do you need them to run faster?
2019-09-22 10:37 AM
They won't run properly at 180 MHz
The TIM nominally run at APB x2
Why do you need them to run faster?
2019-09-22 10:42 AM
I wanted to speed up the peripherals associated with these clocks such as ADC. I am trying to minimize the speed at which each peripheral is operating.
Yes, you are right I read in the datasheet that these are the max frequencies at which these buses can run at.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.