2019-03-15 11:13 PM
Hello,
Micro-controller used : STM32F779NI
Question:
My understanding is that there are two 1.2 V internal regulators.
[1] The regulator that gets enabled by holding BYPASS_REG pin as low
[2] The backup regulator that gets enabled through PWR_CSR1.BRE
Am i right ?
Regards,
Vinoth
Solved! Go to Solution.
2019-03-17 4:03 AM
Yes, these are two mutually independent regulators, but why would that be important?
JW
2019-03-17 4:03 AM
Yes, these are two mutually independent regulators, but why would that be important?
JW
2019-09-21 9:23 AM
Initially i was confused with LPR mode of the regulator with the backup regulator. That's when i had posted this. Thanks.
Regards,
Vinoth
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.