STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f103c8t6 conmunication GY-86

Hello evryone.I'm newbie,I need conmunication stm32f103c8t6 and GY-86 with I2C protocol, read data from Gy-86 with debug console in Keil or SW4STM32.I hope someone help me,I try so lost of and I'm fail.Thanks so much!

PThan.15 by Associate
  • 1146 Views
  • 0 replies
  • 0 kudos

Resolved! Generated binary file size in STM32L4

Is there any specific address location in generated binary file so we can know the size of that binary file?Using this, in the firmware to read the size of binary file from that location and use it in our application.

AP_040 by Senior
  • 24950 Views
  • 65 replies
  • 0 kudos

using Labview VISA to control my STM32 Nucleo-F401RE board.

Hello everyone.I wrote a code for my stm32 Nucleo-L432KC board.Now I'm writing code in LabVIEW in order to send instructions (such as: set the User_selection value in the Nucleo board code) and receive data (such as Temperature variable value in the ...

RFink by Associate II
  • 2842 Views
  • 0 replies
  • 0 kudos

STM32F427 - Calculating VDD from VREFINT - questions

The documentation states that when measuring the CPU's temp, that VREFINT should be used to acquire better accuracy if powered by a battery. So I intent to use VREFINT to determine what the CPU's VDD is without outside components.That's the plan - bu...

Joe.H by Senior
  • 4209 Views
  • 3 replies
  • 0 kudos

In STM32H743zi can HRTIM be used as Time Base generator?

Hi ,I need to toggle a GPIO to create a clock pattern for as much as high frequency as possible , So currently using TIM5 and on overflow callback I toggle the GPIO. The generated clock pulse is around 25 us pulse width, I want to decrease pulse widt...

RSrin by Associate
  • 883 Views
  • 0 replies
  • 0 kudos

Did we discuss STM32 in SO8 yet?

https://www.st.com/content/st_com/en/products/microcontrollers-microprocessors/stm32-32-bit-arm-cortex-mcus/stm32-mainstream-mcus/stm32g0-series/stm32g0x1/stm32g031j6.htmlIt's the same trick as in the STM8s in SO8 - several IO pads bonded together on...

i2c problem

here is the read 16 bytes register codeuint16_t TMP_ReadConfReg(void) { __IO uint16_t RegValue = 0;   /* Enable LM75_I2C acknowledgement if it is already disabled by other function */ I2C_AcknowledgeConfig(LM75_I2C, ENABLE); /*---------------...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.