STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I'm trying to blink one led but two led blinks

Hi,i'm trying to blink only one led. I have a problem with one of four leds. Because as you in my code, i'm trying to blink only 'green led'. But 'blue led' blinks also. #include "stm32f4xx.h" // Device header #include "stm32f4xx_hal...

STM32 trying to get uasart to transmit

Hello, I wanted to upgrade my simple blinky program with the usart 2, so that it sends a simple 'B' over the serial port to my PC. I am using a Nucleo-F334R8. In the datasheet it says usart2 is connected with the USB port.Here is my code, that is not...

Facing issue while flashing code in STM32H745 Disco board?

Hi , I am trying to flash my code of GPIO toggle into the STM32H745 Disco board,but it is giving the error .While building the project I have seen an error "GPIO_CM4\GPIO_CM4.sct(7): error: L6235E: More than one section matches selector - cannot all...

psiva.13 by Associate II
  • 1100 Views
  • 0 replies
  • 0 kudos

The question pertains to maximum rise time specification for STM32L151CC OSC32_IN when Low-speed external user clock is generated from an external source.

The question pertains to maximum rise time specification for STM32L151CC OSC32_IN when Low-speed external user clock is generated from an external source. This specification, according to the datasheet, is 10 nano seconds. This seems unreasonably fas...

faizal by Associate
  • 782 Views
  • 0 replies
  • 0 kudos

STM32H753AI Recommended Footprint

Hello,In the STM32H753AI datasheet, there are footprint guidelines for all the packages, except for the UFBGA169 (see attached image).Has anyone built a board with this package? Where did you find any info on this type of package?Is there a database ...

Yan Rosh by Associate II
  • 3031 Views
  • 3 replies
  • 0 kudos

I2C Library for PCA9685 won't work

I'm creating an I2C library for PCA8596 to control servos using STM32F4 Discovery as master. I already checked the PCA using arduino, and it worked. It also compiled well and can be uploaded.The problem is the SCL and SDA from the stm didn't generate...

Uwii by Associate
  • 1503 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.