AN4861 for 'H7
ST,Please update AN4861 for 'H7Please link to AN4861 from the 'H7 product folder webpagesPlease fix links to AN4861 on forum - those given by Amel and Imen are usually broken, you can find them by searching for DM00287603Thanks,JW
Ask questions, find answers, and share insights on STM32 products and their technical features.
ST,Please update AN4861 for 'H7Please link to AN4861 from the 'H7 product folder webpagesPlease fix links to AN4861 on forum - those given by Amel and Imen are usually broken, you can find them by searching for DM00287603Thanks,JW
Hello everyone, I want to work on STM32 series of controller which supports 480MHZ or above clock rate and Auto grade temperature range(I.e Grade0: -40degc to 150degc (or) Grade1:-40degc to 125degc).We found STM32H7 series which supports our applica...
I am witnessing interrupts on EXTI9_5 line which have absolutely no electrical stimulus. I'm seeing this behavior consistently on multiple chips so this isn't a one-off.The GPIO in question (ONE_WIRE_PIN) is PA8.GPIO initialization here:mIRQConfig.Pi...
https://www.st.com/content/ccc/resource/technical/document/reference_manual/c5/cf/ef/52/c0/f1/4b/fa/DM00124865.pdf/files/DM00124865.pdf/jcr:content/translations/en.DM00124865.pdfReferences to OPT instead of OTP
I am using keil to program STM32F103C8 MCU and I have the the library files for GPIO read and write functions but it is not working. There are no errors. I am just not sure about the parameters I am passing to functions. I have attached the code and...
Hi,I ran several test and example projects on the STM32F769 Discovery platform. I would like to reload the original demo firmware. According to the documentation, it should be available from the www.st.com/stm32f7-discovery webpage but I cannot find ...
Here is my boardhere my clock settingI use CuceMxIDE, here my RTC settingif AsynchPrediv = RTC_AUTO_1_SECOND;rtc take very long time to increase one second. I try some value, and choose 50 and seem the time count rightAsynchPrediv = 50;but I'm not su...
STM32F205 uses the TIM_DMA_Update event loop of timer 8 to trigger DMA2 transport, which moves 5 data from test_data to dest_arr at a time.Using DMA2_Stream1_Channel7, start these two functions in the main program, configure DMA and TIM8, and then ob...
This project uses STM32Cube_FW_H7_V1.3.2.On STM32H7 I'm using DMA for SPI transfer. I use SPI1 and SPI4, both in D2 domain, together with RAM_D2.In the linker file I added:.dma_buffer : { . = ALIGN(4); *(.dma_buffer) } >RAM_D2The ...
Please can you help me. I cannot use the HAL as I have to write an ultra low power/ minimalist application. I need to Tx/Rx a few bytes over I2C3 . I have set it up as below but I do not get any interrupts, either event or errors. Can you tell me wh...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.