2019-09-12 4:21 AM
Hello,
In the STM32H753AI datasheet, there are footprint guidelines for all the packages, except for the UFBGA169 (see attached image).
Has anyone built a board with this package? Where did you find any info on this type of package?
Is there a database of ST footprints I can look at to find this info?
In a similar question, one of the answers led to AN4938 (Getting started with hardware dev....), but there is no specific package information there either...
Thanks in advance,
Yan
2019-09-12 1:06 PM
stm32l4a6 has a similar UFBGA169 package, and I see it's data-sheet has a recommended footprint for a single pad, which is more than you got in your data sheet. Maybe you could build something from that?
But I think this is something you will have to discuss with your pcb house.
I have resorted to stacked via-in-pad to route enough tracks out of an ST WLCSP100 package. Not cheap but I couldn't see how to get the inner tracks out.
Hope this helps,
Danish
2019-09-14 8:32 AM
Thanks for the answer, I saw that datasheet as well, just wanted to make sure that it's indeed the same package...
Yan
2019-09-27 9:35 AM
Hi @Yan Rosh ,
A request is tracked internally to add "UFBGA169 recommended footprint" for STM32H7 datasheets where this package is available.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.