STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G070 Internal RTC Wake Up Interrupt hangs. After few iterations rtc wake up interrupt is hangs. Help will be appreciated.

  if(low_power_mode == 1)  {    standby(10);    HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);      }void standby(int seconds) { /* Clear all related wakeup flags*/  __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF2);  rtc_set_wake_up_timer_s(seconds); HAL_PWR_Enter...

Frequency precision when generating sine wave with DAC

I am currently developing on a NUCLEO-G071RB board and I need to generate sine waves with frequencies in the range 1Hz - 11kHz. My project requires the step between the frequencies to be 1Hz. It doesn't have to be precisely 1Hz but it has to be close...

JMSuckow by Associate
  • 2500 Views
  • 2 replies
  • 0 kudos

QUADSPI indirect-read only

Chip: STM32G474I have a ADC chip that offers SPI-compatible interface, it could achieve below functions in picture.I tried use QUADSPI to achieve that without instruction, address, alternate, dummy, but only DATA with indirect-read mode, but couldn't...

0690X00000AqrviQAB.png 0690X00000AqrvxQAB.png

How to include arm_math in h745 dual core project

Hello, I'm trying to use arm_math.h in the m4 core of an stm32h745, but i get a bunch of really weird errors that seem to indicate that somehow the project configuration is wrong? I set the project properties to Debug_CM4 ( active ) and define CORE_C...

RMcCa by Senior II
  • 1605 Views
  • 4 replies
  • 0 kudos

Arm assembler - branch by a programmable amount

I want to manipulate the program counter in an assembler function by branching down a list of instructions by a programmable amount.syntax unified .global myasm myasm: PUSH {R0,R1,r2,r4,R5} ADD R15,#4    is rejected by the assembler.syntax unified ...

PMath.4 by Senior III
  • 5241 Views
  • 12 replies
  • 0 kudos

Is the DMA overstrained? DMA & InputCapture Issues

Hi everyone, my setting looks like this:CPU CLK: 480MHzAHB CLK should be 240MHz (I'm not 100% sure)Timer CLK 120MHzInputCapture Channel: 4 (2 direct, 2 indirect)I generate 8 short pulses each about 30ns. I use 4 InputCaptures to read those pulses. 2 ...

Programming STM32L4 MCU's internal flash memory with sensor coefficients while keeping the firmware memory section intact

Hello,This is the first time I am using the STM32 MCU.I would like to know how can I re-flash a certain section of the internal flash memory (eg 1000h ~ 1200h) with NEW sensor coefficients while keeping the already flashed MCU firmware intact.Can I u...

GDarr by Associate II
  • 4082 Views
  • 7 replies
  • 0 kudos

Selecting a STM32 MCU

Hi Thank you for having me here! I come from the AVR-Mega community and wondering about selecting a STM32 MCU. I needed more time to process between my input capture and USART and HDLC processing. Which MCU have 4 timers and input/output capture avai...

Donnie B by Associate II
  • 3979 Views
  • 7 replies
  • 0 kudos

STM32f105 double CAN receiv problem

on stm32f105 launched CAN. With the transfer of messages, there were no questions, but there were questions about receiving messages from two CAN.the code is responsible for processing the messagevoid HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeD...

AFoki by Associate
  • 1518 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.