2019-03-05 8:14 AM
on stm32f105 launched CAN. With the transfer of messages, there were no questions, but there were questions about receiving messages from two CAN.
the code is responsible for processing the message
void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan)
{
HAL_CAN_GetRxMessage(&hcan2, CAN_RX_FIFO0, &RxHeader, RxData);
HAL_CAN_GetRxMessage(&hcan1, CAN_RX_FIFO0, &RxHeader, RxData);
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_15);
}but this code works both on the message from can1, and on messages from can2.
As a result, I do not understand from which of the kans this message came.
How to divide, what would be separately messages from can1 and can2?
2019-03-06 4:32 AM
void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan)
{
switch((uint32_t)hcan->Instance)
{
case (uint32_t)CAN1:
/* CAN1 Process */
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_15);
HAL_CAN_GetRxMessage(&hcan1, CAN_RX_FIFO0, &RxHeader, RxData);
TxHeader.StdId=RxHeader.StdId;
TxHeader.DLC = RxHeader.DLC;
TxHeader.IDE = RxHeader.IDE;
HAL_CAN_AddTxMessage(&hcan2, &TxHeader, RxData, &TxMailbox);
break;
case (uint32_t)CAN2:
/* CAN2 Process */
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_15);
HAL_CAN_GetRxMessage(&hcan2, CAN_RX_FIFO0, &RxHeader, RxData);
TxHeader.StdId=RxHeader.StdId;
TxHeader.DLC = RxHeader.DLC;
TxHeader.IDE = RxHeader.IDE;
HAL_CAN_AddTxMessage(&hcan1, &TxHeader, RxData, &TxMailbox);
break;
}
}This is code solved my problem
2019-10-24 7:32 PM
hi there
can you post the HAL_CAN_ActivateNotification section of your code?
im having problems to determine how to activate CAN1, CAN2 and CAN3 reception interrupt.
if (HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK)
{
HAL_UART_Transmit(&huart3, (uint8_t *)"\n\rCAN1_IT_init_ERROR", 20, 10);
Error_Handler();
}i have this implementation for hcan1 but it doesnt works for hcan2
thanks in advance
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.