STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L475 Setting the RTC to 24 hour mode

I am using a STM32L475 and plan to also use an STM32L451 processor, I am having trouble setting the RTC so that its in 24 hour mode. According to the datasheet setting a 0 to bit 22 of RTC_TR should set it into 24 hour mode but this does not seem to ...

PHedl by Associate
  • 1427 Views
  • 1 replies
  • 0 kudos

The procss of using SPI slave with dma

Hi I am fairly new to SPI slave with dma on a microcontroller, I am wondering in firmware what is the process of implementing it? I have set spi1 up as spi slave and assign dma streams to it in the cubeide, but now that it is set up, how is the data ...

This is Horrible experance! It's taken me an hour just to get this far. I can't find anyone to call on this question. The number they have for support is out of service, and any atempt to find a number to call just sends back to the number.

If anyone has a working support number would be a big help.  My Question is on the STM32F411 the data sheets state many of the lines are FT 5 volt t​olerant, other team members don't believe this and want to use level shifters, they believe as many l...

MPoll.961 by Associate II
  • 3985 Views
  • 8 replies
  • 0 kudos

mbedtls handshake failed 0x7780

Hey,I tried the SSL_Client mbedtls example program for the STM32f7 and I get following error:Handshake failed 0x7780Im trying to connect to a cloudflare server via https. Any ideas what the problem could be?thanks in advance

Anon767 by Associate II
  • 1939 Views
  • 1 replies
  • 0 kudos

Connecting 2 16-bit SDRAM as one 32-bit SDRAM

Simple question: is this possible without additional HW logic? I have these two 16-bit SDRAMs and I'd hate to use just one of them or to use them as measly two 16-bit SDRAMs. I think I've browsed through all 3200+pages of reference manual and couldn'...

Slina by Associate III
  • 3732 Views
  • 7 replies
  • 0 kudos

SPI - configure mode 0 (clck pol 0, phase 0) but the output is mode 2 (clck pol 1, phase 0) , with clock idle high

Hi all, I have a STM32F091CC and am using SPI2 on PortB, Pin 13-15.I configure polarity=0 and phase=0, but the trace in logic analyzer and oszi shows that the clock is idle high. I have already tried pullup, pulldown and nopull at CS pin, but with n...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.